In built secured memory to store certificates

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In built secured memory to store certificates

2,127件の閲覧回数
abdulredwan
Contributor III

Hi Team,

We are using imx8qm platform where we need around 4k of SECURED memory in built to store certicates which needs to be preserved on hard as well as soft reset

Please suggest

タグ(3)
0 件の賞賛
返信
5 返答(返信)

2,067件の閲覧回数
abdulredwan
Contributor III

Hi....anybody can help with more information wrt to the source modules pls

0 件の賞賛
返信

2,067件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Abdul,

Please more detail in your question if the question is you can interface secure memory is yes.

Regards

0 件の賞賛
返信

2,067件の閲覧回数
abdulredwan
Contributor III

Thanks Bio_TICFSL

We just want to know since its only 4KB of Memory required to store the certificates does i.MX8 has any memory internally which we can be used for this purpose instead of having an external EEPROM for storing those certificates

Thanks

AMR

0 件の賞賛
返信

2,067件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Abdul,

Internal RAM can be used if you have no plan to use other peripheral and security of i.MX8.

Regards

0 件の賞賛
返信

2,067件の閲覧回数
abdulredwan
Contributor III

Thanks Bio_TICFSL

U mean to say SECO RAM/ROM or any other internal memory. As we said before certificates should be stored persistently on hard/soft reset. Could you guide us to the respective source in the android source code which we can explore - if there are relative post/docs would also be helpful to us

0 件の賞賛
返信