Imxrt1021 iperf freertos throughput.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imxrt1021 iperf freertos throughput.

1,923 Views
Rp777
Contributor I

Hi,

I am testing with the iperf example on imxrt1021 through ethernet.

When using bare-metal example i am getting upto 90 - 95mbps speed.

Where as when testing with freertos i am able to achieve upto 5mbps only.

I tried increasing the TCP_WND(set it to maximum (65535)) and increased the  TCPIP_THREAD_PRIO priority(default was 8 reduced until 4), even increased the PBUF_POOL_SIZE as well.

 

Can anyone give any pointers on this?

What would be the maximum throughput we can expect using freertos?

Labels (1)
0 Kudos
Reply
2 Replies

1,903 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Rp777:

 

Don't test the performance before.  But you can refer to below article for maximizing lwip throughput.

https://lwip.fandom.com/wiki/Maximizing_throughput

 

Regards

Daniel

0 Kudos
Reply

1,893 Views
Rp777
Contributor I

Thank you for the reference @danielchen will look into it.

0 Kudos
Reply