Imx8x qt5 qml gstreamer to display camera video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8x qt5 qml gstreamer to display camera video

5,560 Views
songhongliang
Contributor II

HI

I am using QT5's qml and gstreamer to render camera images, but my CPU and memory usage are very high, but when I use gst-launch-1.0 to display camera real-time images, the CPU and memory usage are very low. In addition, when qml displays the camera, it often reports an error. The log is in the attachment.

0 Kudos
Reply
6 Replies

5,500 Views
malik_cisse
Senior Contributor I

backend:


/* called when the appsink notifies us that there is a new buffer ready for
 * processing */
GstFlowReturn Gstpipeline::newSampleCallback2 (GstAppSink *appsink, gpointer user_data)
{
    GstSample *sample;
    GstBuffer *buffer;
    GstMapInfo info;  

    /* get the sample from appsink */
    sample = gst_app_sink_pull_sample (GST_APP_SINK (appsink));
    buffer = gst_sample_get_buffer (sample);

    gst_buffer_map( buffer, &info, (GstMapFlags)(GST_MAP_READ) );

    //do something with the buffer. E.g, send it to AI NPU unit
    //.....

    gst_buffer_unmap(buffer, &info);

    /* we don't need the appsink sample anymore */
    gst_sample_unref (sample);

    return GST_FLOW_OK;
}

int Gstpipeline::gstpipelineInit()
{
    GError *error = NULL;
    gchar *descr;
    GstStateChangeReturn ret;    

    qInfo() << "gstpipelineInit()";

    /* Initialize GStreamer */
    gst_init (NULL,NULL);

#if 0
    descr = g_strdup_printf ("v4l2src device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw,width=3840,height=2160 ! "
                         "videocrop name=video_crop ! imxvideoconvert_g2d ! glimagesink rotate-method=3 sync=false name=sink ");
#endif

#if 0
    descr = g_strdup_printf ("v4l2src name=video_source device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw, width=3840,height=2160 ! tee name=t "
                         "t. ! queue ! imxvideoconvert_g2d name=g2d rotation=3 ! video/x-raw, width=480, height=800 ! appsink name=app_sink1 max-buffers=2 drop=True "
                         "t. ! queue ! appsink name=app_sink2 max-buffers=2 drop=True ");
#endif

#if 1
    descr = g_strdup_printf ("v4l2src name=video_source device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw, width=3840,height=2160 ! "
                         "videocrop name=video_crop ! imxvideoconvert_g2d rotation=3 ! video/x-raw, width=480, height=800 ! appsink name=app_sink1 max-buffers=1 drop=True  ");
#endif

#if 0
    descr = g_strdup_printf ("v4l2src name=video_source device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw, width=3840,height=2160 ! "
                         "videocrop name=video_crop ! imxvideoconvert_g2d ! video/x-raw, width=800, height=480 ! intervideosink sync=false  ");
#endif

#if 0
    descr = g_strdup_printf ("v4l2src name=video_source io-mode=5 device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw, width=3840,height=2160 ! "
                         "videocrop name=video_crop ! imxvideoconvert_g2d ! video/x-raw, width=800, height=480 ! interpipesink name=src_1 sync=false ");
#endif

#if 0
    descr = g_strdup_printf ("v4l2src name=video_source device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw, width=3840,height=2160 ! tee name=t  "
                         "t. ! queue ! imxvideoconvert_g2d name=g2d ! video/x-raw, width=800, height=480 ! interpipesink name=src_1 sync=false "
                         "t. ! queue ! appsink name=app_sink2 max-buffers=2 drop=True ");
#endif

#if 0
    descr = g_strdup_printf ("v4l2src name=video_source device=/dev/v4l/by-path/platform-vvcam-video.0-video-index0 ! video/x-raw, width=3840,height=2160 ! tee name=t  "
                         "t. ! queue ! imxvideoconvert_g2d name=g2d ! video/x-raw, width=800, height=480 ! interpipesink name=src_1 sync=false "
                         "t. ! queue ! appsink name=app_sink2 max-buffers=2 drop=True ");
#endif

    data.pipeline = gst_parse_launch (descr, &error);
    if (error != NULL)
    {
      qDebug() << "launch_gst_pipeline: could not construct gstreamer pipeline:" << error->message;
      g_clear_error (&error);
      return 0;
    }    

    data.v4l2src = gst_bin_get_by_name( GST_BIN( data.pipeline), "video_source");

    data.videocrop = gst_bin_get_by_name( GST_BIN( data.pipeline), "video_crop");
    g_object_set(data.videocrop, "left", left_crop, "right", right_crop, "top", top_crop, "bottom", bottom_crop, NULL);

    //data.g2d = gst_bin_get_by_name( GST_BIN( data.pipeline), "g2d");

#if 1
    /* we use appsink in push mode, it sends us a signal when data is available
    * and we pull out the data in the signal callback. We want the appsink to
    * push as fast as it can, hence the sync=false */
    data.appsink1 = gst_bin_get_by_name (GST_BIN (data.pipeline), "app_sink1");
    g_object_set (G_OBJECT (data.appsink1), "emit-signals", TRUE, "sync", FALSE, NULL);
    g_signal_connect (data.appsink1, "new-sample", G_CALLBACK (newSampleCallback1), this);
    //gst_object_unref (data.appsink1);
#endif

#if 0
    data.appsink2 = gst_bin_get_by_name (GST_BIN (data.pipeline), "app_sink2");
    g_object_set (G_OBJECT (data.appsink2), "emit-signals", TRUE, "sync", FALSE, NULL);
    g_signal_connect (data.appsink2, "new-sample", G_CALLBACK (newSampleCallback2), this);
#endif
    ret = gst_element_set_state(data.pipeline, GST_STATE_PLAYING);
    if (ret == GST_STATE_CHANGE_FAILURE)
    {
        qDebug() << "launch_gst_pipeline: Unable to set the gstreamer pipeline to the playing state.";
        gst_object_unref (data.pipeline);
        return 0;
    }

    return 1;
}


QML frontend

import QtQuick 2.6
import QtQuick.Controls 1.4
import QtMultimedia 5.4
import QtQuick.Window 2.12

Window {
id : cameraUI
visible: true
color: "black"
property real zoomValue : 1.5
property int zoomCntr : 0
property int illuScenNr: 3
property string snaptext: ""
property bool showMenu: false

Item { //needed for keypad event handler
anchors.fill: parent
focus: true

/*MediaPlayer {
id: mediaplayer
autoPlay: true
//source: "gst-pipeline: intervideosrc ! queue ! qtvideosink sync=false"
source: "gst-pipeline: interpipesrc is-live=true listen-to=src_1 ! queue ! qtvideosink sync=false async=false"
//videoOutput: [v1, v2]
}

VideoOutput {
id: output
anchors.fill: parent
source: mediaplayer
focus : visible // to receive focus and capture key events when visible

transformOrigin: Item.Center
orientation: 90
MouseArea {
anchors.fill: parent
onClicked: {
showMenu = true
}
}
}*/

//preview camera on LCD
VideoOutput {
source: frameProvider
anchors.fill: parent
focus : visible // to receive focus and capture key events when visible
//transformOrigin: Item.Center
//orientation: 90
//fillMode: VideoOutput.PreserveAspectCrop
MouseArea {
anchors.fill: parent
onClicked: {
showMenu = true
}
}
}

0 Kudos
Reply

5,531 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @songhongliang,

I hope you are doing well.
 
This issue could be due to Qt might not have hardware acceleration components enabled in the back end and this results in high CPU usage.
 
Please refer to the below link for how to use GPU resources in a Qt application
 
Please try using cpuidle.off=1 in bootargs which can reduce the cpu loading while testing with iperf.
 
Please try building imx-image-full with the latest BSP as suggested in the 5.6.2 XWayland image on i.MX 8QuadXPlus MEK in i.MX Yocto Project User's Guide
 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply

5,369 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @songhongliang,

I hope you are doing well.

waiting for your response to above comments

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply

5,535 Views
malik_cisse
Senior Contributor I

Hi,

It would be good if you could provide more details about your pipeline.

From your description I understand you use QT QML Mediaplayer like this:

  MediaPlayer {
        source: "gst-pipeline: udpsrc port=5000 ! h264parse ! avdec_h264 ! videoconvert ! qtvideosink"
        autoPlay: true
    }

This is bad and deprecated.

You could instead implement a regular Gstreamer pipeline using native API (equivalent to gst-launch-1.0 ... command) and fead qml via "intervideosink" or "interpipesink" elements. 
In qml you could Mediaplayer just to render "intervideosrc" video through "qtvideosink".
One can completely bypass mediaplayer and pass video to QML videooutput. There is sample code on the web. I implemented this myself.
Alternatively you could use "qmlglsink"
https://gstreamer.freedesktop.org/documentation/qmlgl/qmlglsink.html?gi-language=c

0 Kudos
Reply

5,156 Views
meifangchang
Contributor I

"Hello, I am using qmlglsink to play the camera, but the image is tearing. Do you know how to solve it?"

0 Kudos
Reply

5,522 Views
songhongliang
Contributor II

Hi

As you said, I use something like  gst-pipeline. Can you show me your routine? I now want to realize simultaneous playback of 3 local camera images.

Thanks!

0 Kudos
Reply