Imx8dx CAN sampling point settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx8dx CAN sampling point settings

2,772件の閲覧回数
songhongliang
Contributor II

Where to change the sample point settings

0 件の賞賛
返信
4 返答(返信)

2,771件の閲覧回数
songhongliang
Contributor II

flexcan驱动默认的采用点是75%吗

 

0 件の賞賛
返信

2,753件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @songhongliang 

I hope you are doing well.

1)Where to change the sample point settings?
One can change the settings of the CAN device properties.
ip link set DEVICE type can

"bitrate 125000 sample-point 0.875"
by this argument, one can set the bitrate and optionally one can set the sample-point

after Please verify the values by
ip -details -statistics link show can0

For more details please refer to the can.rst file in the Linux source code.
<source_code>/Documentation/networking/can.rst

2)Is the default adoption point of the flexcan driver 75%?
Can you please kindly elaborate on this term & share more detail on it?

Thanks & Regards.

Sanket Parekh

0 件の賞賛
返信

2,737件の閲覧回数
songhongliang
Contributor II

In imx8dx, if I don't set sample point 0.875, what is the default sample point

0 件の賞賛
返信

2,730件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @songhongliang ,

I hope you are doing well.

->One can check by default statistics by the below give the command.
ip -details -statistics link show can0

Thanks & Regards,

Sanket Parekh

0 件の賞賛
返信