Imx7d sabre, u-boot and GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx7d sabre, u-boot and GPIO

2,176 次查看
jensalsig
Contributor I

Hi

I'm trying to use one the two switch on the Sabre board in u-boo to select the boot device, either boot from SD-card or network.

But I'm stuck at the gpio part. I'm not able to read the value of either of the switches.

According to Definitive GPIO guide - Studio Kousagi Wiki​ the iopin number will be 138 for Sw3 (usr_bt1). I know that the source calculates on a imx6 but I assume that the calculations for the iopin is the same on the Imx7

I have tried, in u-boot:

"gpio i 138"

but the value returned is always 0.

I have also browsed through the u-boot code, but I was not able to find anything regarding gpio in the imx7. This leads me to believe that it isn't configured. Is this true? And if not are there any example/guides on how to enable it?

/Jens

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,303 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jens

mentioned link described gpios in linux, while uboot is not linux.

In u-boot one can just write/read to processor registers using commands md,mw.

Also please use i.MX7D Reference Manual sect.8.2 IOMUX Controller (IOMUXC),

sect.8.3. General Purpose Input/Output (GPIO)

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复