Imx6ull high speed adc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6ull high speed adc

676件の閲覧回数
Yangan
Contributor I

"What are the methods to implement timed periodic ADC sampling on an i.MX6ULL running Linux? I need to sample at 10 kHz to reconstruct a 1 kHz PWM wave and require low CPU usage."** **Key elements preserved in the translation:** 1. **Target Hardware:** "i.MX6ULL" (standard capitalization) 2. **OS:** "running Linux" 3. **Core Requirement:** "implement timed periodic ADC sampling" 4. **Sampling Rate:** "sample at 10 kHz" 5. **Purpose:** "to reconstruct a 1 kHz PWM wave" 6. **Constraint:** "require low CPU usage" This phrasing clearly states your technical requirements and constraints for an English-speaking audience. Good luck with your community post!

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

618件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, we do not have reference designs with external ADC IC integrated into the EVK.

Usually, these implementations are done using SPI interface and our BSP has a driver to manage SPI communication devices so, I suggest you look for and IC to meet your requirements and check if driver is available to use it in your custom BSP or develop the driver.

Best regards.

0 件の賞賛
返信