Imx6ul spi clock interval

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6ul spi clock interval

3,562件の閲覧回数
jieh朱
Contributor III

Hello!

   I am using imx6ul

   The kernel version is linux4.1.15

   I configured the device tree and kernel and tested it with Documentation/spi/spidev_test.c

   However, I set up an 8-bit transfer. After the clock has finished transmitting the 8-bit byte, there will be a time interval and then the clock will be sent. As shown below, I should modify it there to modify the size of the interval.

pastedImage_1.png

5 返答(返信)

3,321件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jiehuai


I am afraid it is not possible to decrease time interval, as it is caused

by processor internal bus delays. For improving throughput one can increase

BURST_LENGTH parameter in ECSPIx_CONREG register or try with/or without

sdma:

                ecspi1: ecspi@02008000 {..
                    dmas = <&sdma 3 7 1>, <&sdma 4 7 2>;
                    dma-names = "rx", "tx";

imx6ul.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,321件の閲覧回数
jieh朱
Contributor III

Thank you for your reply
   I use dma transfer or pio transfer, it will have the above problem
   How should ECSPIx_CONREG register be configured?
   I saw it in IMX6ULRM
   Is it possible to configure this register?

   pastedImage_1.png

      How to configure if I can. I didn't find the location of this register in the kernel.
Thank you

0 件の賞賛
返信

3,321件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

linux driver does not use it, so it is in reset state, so seems there is no

way to decrease it more.

Best regards
igor

0 件の賞賛
返信

3,321件の閲覧回数
dahyunkim
Contributor I

jieh朱‌

Hello, 

I had a same problem in imx6qdl and I have to reduce the interval of the spi clock.(actually, I have to get no interval in spi clock)

I am wondering the way can modify the interval of the spi clock.

Is the interval time related in Clock Controller Module? 

0 件の賞賛
返信

3,321件の閲覧回数
jieh朱
Contributor III

Thank you for your reply

   Can I modify the interval of the spi clock? Or is the interval time cpu design can not be modified?

0 件の賞賛
返信