Imx6q receiving data through ssi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6q receiving data through ssi

2,983 Views
hsl
Contributor I

Hello everyone:

I would like to ask:
Imx6q connects to the external i2s signal through audmux3. How can I configure the i2s data to be received through the ssi interface?

Just like this connection, there is no ssi codec, only three signal lines are connected to audmux:

pastedImage_1.png

Thank you~

Labels (1)
0 Kudos
Reply
2 Replies

2,899 Views
igorpadykov
NXP Employee
NXP Employee

Hi H

in general such connection is possible, example of ssi-audmux programming

one can find in AN2628 Programming Audio Applications

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,899 Views
hsl
Contributor I

Hi,Igorpadykov:

Thank you for your reply!
The AN2628 programming audio application you said in the reply did not find it. The link is just a chip introduction manual.
Now I am connected like this, but how do I configure it to read the i2s signal? Seeking advice!
Thank you

0 Kudos
Reply