Imx6q gpio interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6q gpio interrupt

1,394 Views
hsl
Contributor I

Hi,Everyone:

Imx6q gpio interrupt, 3MHz frequency can not respond in time?

For example, if the level of the IO port is read in the interrupt, will there be data missing?

thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,259 Views
igorpadykov
NXP Employee
NXP Employee

Hi H

seems it should work in not heavy loaded linux applications,

suggest to test with linux minimal configurations.

Linux documentation for building images can be found on

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply