Imx6q android4.4 open GPU so library application slow question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6q android4.4 open GPU so library application slow question

1,477 Views
sean_xiao1
Contributor I

The following is the log. When the application is opened, the system loads the GPU library, which takes about 10s.

06-30 09:11:58.640 D/libEGL  ( 2227): loaded /system/lib/egl/libEGL_VIVANTE.so

06-30 09:12:01.550 W/audio_hw_primary( 1290): do_out_standby... 1093698504

06-30 09:12:08.070 D/libEGL  ( 2227): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so

06-30 09:12:08.150 D/libEGL  ( 2227): loaded /system/lib/egl/libGLESv2_VIVANTE.so

06-30 09:12:08.220 E/BufferQueue( 1287): [com.zl.my/com.zl.my.MainActivity] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

06-30 09:12:08.230 D/OpenGLRenderer( 2227): Enabling debug mode 0

06-30 09:12:08.300 I/ActivityManager( 1654): Displayed com.zl.my/.MainActivity: +9s946ms

06-30 09:12:08.300 E/WindowManager( 1654): Starting window AppWindowToken{41d9d8a8 token=Token{41d9cba0 ActivityRecord{41f4d328 u0 com.zl.my/.MainActivity t4}}} timed out

This is a problem found in the mass production equipment. The customer does not upgrade the kernel system, but only upgrades the GPU Driver to solve the problem. Is there a patch available?

  Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,436 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sean

android 4.4 is old release not more supported, recommended to migrate to new

releases described on

Android OS for i.MX Applications Processors | NXP 

Support for old releases is provided with extended support of

Professional Engineering Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply