Imx6 default SD Card image.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 default SD Card image.

1,570件の閲覧回数
SumitVaidya
Contributor II

Hi,

 

I bought IMX6 evaluation kit and was able to boot evaluation board with SD Card provided in the package. After that I tried to put my own u-boot.bin and uImage on the SD Card to verify it boots properly.

 

I get following error when I boot.

 

In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:19:b8:00:e9:e9
FEC0 [PRIME]
Hit any key to stop autoboot:  0
Card did not respond to voltage select!
mmc0(part 0) is current device
MMC: block number 0x1 exceeds max(0x0)
** Can't read from device 0 **

** Unable to use mmc 0:1 for fatload **
** Bad partition 1 **
mmc1 is current device
reading /6q_bootscript

** Unable to read "/6q_bootscript" from mmc 1:1 **
Loading file "/6q_bootscript" from mmc device 1:1 (xxb1)
** File not found /6q_bootscript

 

I am looking where can I find this 6q_bootscript file. As I lost the default image on SD card is there a way to recover this image? I searched on freescale website but did not find any documentation for this.

 

Regards,

Sumit

タグ(2)
0 件の賞賛
返信
1 返信

1,087件の閲覧回数
SumitVaidya
Contributor II

I was able to boot this board after installing back these missing files. This is closed now.

 

Regards,

Sumit

0 件の賞賛
返信