Hi,
I have a imx6 sabrelite board and I am trying to ping the boards IP from the PC and It works fine, similarly I could ping PC from the imx6 board.
I have a Vayu EVM board and I trying to ping this board from the imx6 and it could not and the same when tried other way.
this is my result when tried ping
Ping form imx6
ping 172.16.7.117
PING 172.16.7.117 (172.16.7.117): 56 data bytes
^C
--- 172.16.7.117 ping statistics ---
3484 packets transmitted, 0 packets received, 100% packet loss
ping from j6
ping 172.16.7.123
PING 172.16.7.123 (172.16.7.123): 56 data bytes
^C
--- 172.16.7.123 ping statistics ---
2941 packets transmitted, 0 packets received, 100% packet loss
No reply packets are received,
I also tried sending ethernet and IP packets from imx6 on multicast and could successfully receive in the Vayu board. But when the Vayu board sends the packet the imx socket could not receive. But the same packets from PC could be received by imx6.
Please suggest me of solution! Thanks in advance
Regards,
Sarah Blessie