Imx6 Ethernet link detection problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 Ethernet link detection problem

1,430件の閲覧回数
LArmstrong1985
Contributor III

Hi,

I've an issue on Ethernet with my custom board based on iMX.6 DualLite.

The physical driver is LAN8710 and kernel version  is 4.1.15.

All works fine if I connect board point to point with a PC or using a switch/router.

If a connect two board point to point among themselves instead, the ethernet link is detected only if is connected at startup. If cable is disconnected at startup or if a detach and reattach the cable afterwards, link is not detected. Last row on dmeg is this: 

fec 2188000.ethernet eth0: Link is Down

What could be the cause? Are you aware of any problems of this kind, perhaps related to the physical driver, which have been resolved with patches or in higher versions of the kernel?

0 件の賞賛
返信
0 返答(返信)