Dear NXP Support,
I am currently working on a design based on the i.MX6 processor (most likely Dual). Downloaded the SABRE_AI and SABRESDB / SABRESDP platform design files (as a good starting point for my design) and tried to import the SCH-s into the Altium tool, however, for all the designs, the OrCAD pages with TEXT ONLY were preventing conversion for some reason (although there was no problem to do that for some other OrCAD schematics, but without a lot of text). May you do me a favor and at least for one of the designs (e.g., SABRESDB) send me the DSN file without these text-only pages, please?
Another option might be saving the same design in the older (e.g. 16.2) OrCAD revision...
May you also, for the same SABRESDB design, convert its existing layout from the modern BRD to the older Allegro ALG format, please? Or PADS? – The Altium tool I am using can import these formats.
I do understand that the most likely reason for holding Cadence files only is that very popular Cadence, not Altium, is the official design tool of the i.MX6 support team; however, Altium is a popular tool, too, and I am sure the other customers will also benefit from your reply.
Sincerely yours, Naoum Gitnik.
已解决! 转到解答。
Please find attached the schematic of the i.MX6Q SABRE SD board converted to the OrCAD v.16.2 format.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please find attached the schematic of the i.MX6Q SABRE SD board converted to the OrCAD v.16.2 format.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Please use the following :
I would like the LAY-27962_C.brd file in ASCII (ALG) or already imported into Altium Designer
https://community.nxp.com/message/631345
i.MX6SDP Design Files in Altium format?
[i.MX6] SABRE-SDB design files for Altium
https://community.nxp.com/message/593058
Regards,
Yuri.
Hello Yuri,
thank you for the links.
In fact, I am looking how to convert Allegro files for the QoriQ IoT Gateway and the QoriQ Tower Module.
I have .dsn, .brd, but no .alg file.
The project in Altium format will also help.
Best regards,
Dusan.