Hi,
We try to play a video by "Cactus Player" on android JB4.3-1.1.1-GA
It can play but after bluetooth A2DP connected it will lag in every 2~3 seconds.
Have anyone the same issue. How to solve?
Follow is the information about the video,
- MPEG-4 (QuickTime)
- Video info : 8308 Kbps, 1280*720(16:9) and 29.970 (29970/1000) fps, AVC(High@L5) (CABAC/16 Ref Frames)
- Audio info : 96Kbps, 48.0KHz, Stereo AAC(LC)
Test platform:
1. CPU: i.MX6Q
2. OS: android_jb4.3_1.1.1-ga
3. boot from eMMC.
Test step:
1. Bluetooth A2DP connected.
2. Using 'Cactus Player' open TEST.mov file from internal SD card.
3. Video have lag every 2~3 seconds, but the audio output is normal.
Regards,
Peter
Hello Peter,
Can you please tell me if you did any changes to the BSP?, video will run normal if A2DP is not enabled?
Hi Sergio Solis,
If you do not enable A2DP video playback is normal.
We just porting BCM43241 module to BSP.
Thanks,
Peter