Implementing AVB Stack on IMX6 SABRE AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing AVB Stack on IMX6 SABRE AI

4,243 Views
ajayvenkatakris
Contributor II

Is there any open source software available for implementing the AVB stack on the IMX6 Sabre AI board. If available, how can I implement the stack on the board which is running a yocto image.

Labels (3)
1 Reply

2,469 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ajay Venkatakrishnan,

There is not an Open Source implementation of the AVB Stack for the i.MX6 Sabre AI board that I know of. NXP provides an AVB stack tough NXP Professional Services (which is not an Open Source solution)

http://www.nxp.com/products/software-and-tools/run-time-software/professional-services-software-tech...

Some third parties like Harman provide their own implementation of AVB (please note this is also not Open Source) that I believe it’s compatible with the i.MX6 and certificated for Automotive applications.

http://services.harman.com/resources/ethernet-avb-solution

If you wish a simple implementation perhaps the following AVB demo might help. I haven’t tested but it’s a very brief demonstration of AVB and you may be able to build up from there.

https://community.nxp.com/docs/DOC-95578

There are AVB Open Source initiatives like AVNU’s (link below) but there is no i.MX6 Support, you would need to adapt it and the implementation available is limited and does not provide a comprehensive stack.

http://avnu.github.io/Open-AVB/

I hope this information helps!

Regards,