Ibis Model for PMIC PF3000 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ibis Model for PMIC PF3000 ?

2,165件の閲覧回数
wowa
Contributor I

Dear Community,

i want combine the PF3000 with the i.mx6ul. Does exist a Ibis-model for the PF3000 also ? Does it make sense to design

with Ibis ?

Thx and BR

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,070件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Walter

I am afraid such model is not available. In general it makes sense

to use it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,070件の閲覧回数
wowa
Contributor I

Hi Igor,

yes it should makes sense. I got an answer from direct support. That means there is no model available and it would be too expensive cause the win of that result would be too small ......

For the "i.mx6ul" i got the Ibis. For notice for the community here. You can get it only if you have an NDA with NXP.

BR

0 件の賞賛
返信