Ibis Model for PMIC PF3000 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ibis Model for PMIC PF3000 ?

2,166 Views
wowa
Contributor I

Dear Community,

i want combine the PF3000 with the i.mx6ul. Does exist a Ibis-model for the PF3000 also ? Does it make sense to design

with Ibis ?

Thx and BR

Labels (4)
0 Kudos
Reply
2 Replies

2,071 Views
igorpadykov
NXP Employee
NXP Employee

Hi Walter

I am afraid such model is not available. In general it makes sense

to use it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,071 Views
wowa
Contributor I

Hi Igor,

yes it should makes sense. I got an answer from direct support. That means there is no model available and it would be too expensive cause the win of that result would be too small ......

For the "i.mx6ul" i got the Ibis. For notice for the community here. You can get it only if you have an NDA with NXP.

BR

0 Kudos
Reply