ISL79985 with grecorder-1.0 tool has errors.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ISL79985 with grecorder-1.0 tool has errors.

2,492 次查看
joewu_msi
Contributor I

Hi all,


I use iMX6Q with ISL79985 as our development board, and have apply those patches as described  below:
iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP

My BSP is yocto L4.1.15.

I have tried "mxc_v4l2_tvin.out" test application and gst-launch-1.0, and both work fine.

 

But I have some qustions.

when I used Freescale grecorder-1.0 tool to record video, preview is ok, but press "r", then it has the following errors:

case #1: VIDIOC_QBUF: buffer already queued

[INFO]  ringBufferEnable 0, chromaInterleave 0, mapType 0, linear2TiledEnable 0

start recording

[Current Media Time] 000:00:01ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

(grecorder-1.0:759): GStreamer-CRITICAL **: gst_buffer_iterate_meta: assertion 'buffer != NULL' failed

(grecorder-1.0:759): GStreamer-CRITICAL **: gst_buffer_add_meta: assertion 'buffer != NULL' failed

Segmentation fault

               

case #2: Internal data flow error
               

[INFO]  ringBufferEnable 0, chromaInterleave 0, mapType 0, linear2TiledEnable 0

start recording

[Current Media Time] 000:00:01Error: Internal data flow error.

error, post stop message.

process_message: 2

 

Can somebody give me some suggestions?

BRs,

0 项奖励
回复
2 回复数

2,198 次查看
joewu_msi
Contributor I

Hi igorpadykov,

Thank you for help.

After setting the options "--camera_id 0 --video_format 4 --width 720 --height 240 --fps 30", grecorder-1.0 doesn't occur "VIDIOC_QBUF" recording problems.

0 项奖励
回复

2,198 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Joe

if preview is ok but record video fails this may be perfomance

issue as mentioned on threads with similar errors:

imx6q sabre AI board MIPI camera. 

https://community.nxp.com/docs/DOC-328548?commentID=43777#comment-43777 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复