IPU alpha blending

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPU alpha blending

2,535件の閲覧回数
deepanrajanbara
Contributor IV

Hi,

I am using i.Mx6 based processor and my doubt is that.

Is it possible to both display in fb0 and save the output buffer to a file at the same time .

When i tried to do so i get segmentation fault.Is there something that am missing. Can Any one help me as am new to IPU.

Thank you,

Deepanraj.A

2 返答(返信)

2,295件の閲覧回数
art
NXP Employee
NXP Employee

Seems that you can use Gstreamer for that. For more information, please refer to the Chapter 7 "Multimedia" of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,295件の閲覧回数
rogerio_silva
NXP Employee
NXP Employee

Hi,

Usually alpha blending is made on display processor (DP). As the only output of DP is the display, this will not be an option for you.

You could combine the images using VDIC (Video de-interlace) and send the result to display and other memory location. You will need to implement it on kernel, IPU driver.