IMXRT1176 SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1176 SDRAM

2,348件の閲覧回数
Chethanbg
Contributor III

Hi,

We are developing Instrument cluster application for one of our client using RT1176 controller.

We interfaced Winbond SDRAM 8MB (W9864G6KH-6I).We designed PCB and doing board bringup activity.

Below 2 pins are interchanged

From MCU bank select BA0 is connected to SDRAM BA1

From MCU bank select BA1 is connected to SDRAM BA0

This will cause any issue in SDRAM configuration??if it is causing what configuration settings we should change in firmware?

 

Attached is the image of SDRAM sch

 

 

 

 

0 件の賞賛
返信
2 返答(返信)

2,314件の閲覧回数
Chethanbg
Contributor III

Any update on above ticket raised?

0 件の賞賛
返信

2,294件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Chethanbg ,

This is a tough question. We haven't such experience. But I have to say I can't find any reason to oppose it.

 

regards,

Jing

0 件の賞賛
返信