IMXRT1176 M4 Core Slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1176 M4 Core Slow

2,244 Views
ashok2
Contributor I

Hi,

We are working on a custom board based on IMXRT 1176 and facing a problem with the performance of the M4 core in the dual core system.

M7 is configured for 800Mhz

Compiler options -O2

Memory address DTCM - 0x20000000

Memset for 1000 bytes takes 3.8us

Memcpy for 1000 bytes takes 3.8us

M4 is configured for 400Mhz

Compiler options -O2

Memory address DTCM - 0x20000000

Memset for 1000 bytes takes 29us

Memcpy for 1000 bytes takes 27us

We have also attached the detailed analysis report. 

We would like to know the reason for this slow perfomance on the M4 core ?

 

Regards,

Ashok

 

 

 

Labels (1)
0 Kudos
Reply
2 Replies

2,159 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I apologize for the time long being taken, I'm following your case, I'm working on your case, and when I have more information, I will contact you.

Best regards,
Pavel

0 Kudos
Reply

2,202 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I will do a report on that performance, I will not have a response about that because this will involve other departments, thanks for being interested in product NXP.

Best regards,
Pavel

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply