IMXRT1050-EVKB PCB layout file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1050-EVKB PCB layout file

771件の閲覧回数
dbaselt
Contributor I

When designing the PCB layout for the SDRAM interface, the MIMXRT1050 Hardware Development Guide says "Ideally, route all signals at the same length as the EVK board. See the IMXRT1050-EVKB layout to route all signals at the same length (±50 mils)."

However, the EVK board layout is provided as an Allegro binary file (.brd), which can only be opened on a computer that has Allegro installed.

Is the IMXRT1050-EVKB PCB layout available in a format that can be read with Altium Designer, such as an Allegro ASCII file (.alg) or an Altium Designer layout file (.PcbDoc)?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)