IMXQuad 24MHz Oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXQuad 24MHz Oscillator

3,996件の閲覧回数
ramakarishnamar
Contributor I

Hi

I'm using IMX6 Quad processor.

What is the major advantages or disadvantages using External clock source instead internal Oscillator with crystal design.

If power consumption or internal oscillator is the big issue, Can you provide the details about it.

Thanks

Raju

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,517件の閲覧回数
Yuri
NXP Employee
NXP Employee

First, the following general considerations may be helpful.

http://www.differencebetween.net/technology/difference-between-oscillator-and-crystal4/

Next, the following items may be considered when comparing real / available crystals and oscillators :

1.

Cost. Crystals usually are cheaper.  

2.

Package Size. It depends on real considered parts.

3.

Start-up time. It depends on real considered parts.

4.

Additional pins, elements.

Crystals require extra circuitry (capacitors), that can affect the frequency accuracy and stability.

Oscillators require power voltage (and GND), but their accuracy and stability are specified.   

5.

Drive Level – when using an external oscillator its signal level should match

input specs of processor. No need for such considerations for crystal.

0 件の賞賛
返信

2,517件の閲覧回数
ramakarishnamar
Contributor I

Thanks Yuri

The main concern i have is Jitter of 24MHz clock to IMX6.

Currently I'm using SiLAB clock generator IC.

It is very hard to find ~1.1V , 24MHz clock generator IC. So ended up using potential divider to bring down to 1.1V.

This causing big difference in Jitter.

I'm planning going back to internal oscillator of IMX6. But what i heard is , internal oscillator is power hungry.

I'm looking for specific details of power consumption.

Raju

0 件の賞賛
返信

2,517件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to

https://community.freescale.com/docs/DOC-93757

The document, published there,  contains power calculator.

0 件の賞賛
返信