IMX93 EVK Remove Sensor Module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93 EVK Remove Sensor Module

1,307 Views
lykaios1203
Contributor II

Can we remove the sensor module from the IMX93 EVK board?

0 Kudos
Reply
2 Replies

1,277 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @lykaios1203 

yes , i think its no problem to remove it.

B.R

0 Kudos
Reply

1,305 Views
lykaios1203
Contributor II
We would like to connect other I3c device but do not want two device on the same bus, if we remove the sensor module U1001, can the system still boot and is the HW accept this change?
0 Kudos
Reply