[IMX8QXP] Yocto system get stuck when booting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[IMX8QXP] Yocto system get stuck when booting

2,509件の閲覧回数
Chengyu
Contributor I

Hi,

It's my yocto version configuration.

Yocto version: 5.4.24-2.1.0、5.4.70_2.3.6

DISTRO and MACHINE: DISTRO=fsl-imx-xwayland MACHINE=imx8qxpc0mek source imx-setup-release.sh -b imx8qxpc0mek_xwayland

targets: bitbake imx-image-core

using busybox as init manager,modified fsl-imx-preferred-env.inc

VIRTUAL-RUNTIME_init_manager = "busybox"
POKY_DEFAULT_DISTRO_FEATURES += " sysvinit"

I made 2 more partitions on my emmc, rootfs is at mmcblk0p2, and mmcblk0p3、mmcblk0p4 partition will auto mount.

We try to poweroff and boot the IMX8 board over and over again, but when poweroff 700-1000+ times, the system will get stuck without any wrong log print out. We just can't input any character by console. Of course, our application is background running. At first, I just think the reason of system stuck is something wrong is our application, but we notice the system will also get stuck before the app run. Then we stop the app auto start totally, system will still get stuck with very small probability. It will take a long time to recurrence the problem, so we just add some "sync" operation in the init scripts, probability become bigger. System get stuck when poweroff and boot about 1000 times.

We have tried using "mount" command to mount other partitions, but no effect. System works fine when just mount rootfs partition. We also tried using buildroot filesystem using the same partitions, buildroot works just fine after 30000 times booting ...

Chengyu_1-1651139297044.png

sometimes system got stuck before login.

We could not found any similar problem in community, could anyone give me some suggests.

System stuck log is above.

Best regards.

 

 

 

U-Boot 2020.04 (Mar 24 2022 - 10:05:50 +0800)

CPU:   NXP i.MX8QXP RevC A35 at 1200 MHz at 41C

Model: NXP i.MX8QXP MEK
Board: iMX8QXP MEK

BuildInfo:

  - SCFW 4a1654e0, SECO-FW 376e3c15, IMX-MKIMAGE 694c959b, ATF 694c959
  - U-Boot 2020.04

Boot:  MMC0
DRAM:  1022 MiB
MMC:   FSL_SDHC: 0
Loading Environment from MMC... OK
[*]-Video Link 0 (800 x 480)
        [0] dpu@56180000, video
        [1] lvds-channel@0, display
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc0(part 0) is current device
flash target is MMC:0
Net:   No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0(part 0) is current device
** Invalid partition 8 **
26411520 bytes read in 633 ms (39.8 MiB/s)
Booting from mmc ...
96063 bytes read in 14 ms (6.5 MiB/s)

## Flattened Device Tree blob at 83000000

   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 0000000083000000, end 000000008301a73e
Disable clock-controller@59580000 rsrc 512 not owned
Disable dsp@596e8000 rsrc 512 not owned
Disable clock-controller@5a4d0000 rsrc 62 not owned
Disable clock-controller@5ac90000 rsrc 102 not owned

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd042]
[    0.000000] Linux version 5.4.24 (hzsj377@sjgdworkstation) (gcc version 9.2.0 (GCC)) #2 SMP PREEMPT Wed Mar 23 16:47:48 CST 2022
[    0.000000] Machine model: Freescale i.MX8QXP MEK
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 64 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090000000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev0vring0@90000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090008000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev0vring1@90008000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090010000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev1vring0@90010000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090018000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev1vring1@90018000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[    0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '')
[    0.000000] printk: bootconsole [lpuart32] enabled
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x00000000bfffffff]
[    0.000000] NUMA: NODE_DATA [mem 0xbfdfa500-0xbfdfbfff]
[    0.000000] Zone ranges:
[    0.000000]   DMA32    [mem 0x0000000080200000-0x00000000bfffffff]
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080200000-0x0000000083ffffff]
[    0.000000]   node   0: [mem 0x0000000086200000-0x0000000087ffffff]
[    0.000000]   node   0: [mem 0x0000000090020000-0x00000000901fffff]
[    0.000000]   node   0: [mem 0x0000000090500000-0x0000000091ffffff]
[    0.000000]   node   0: [mem 0x0000000094c00000-0x00000000bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000000bfffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] percpu: Embedded 23 pages/cpu s55832 r8192 d30184 u94208
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 204844
[    0.000000] Policy zone: DMA32
[    0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw
[    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 719744K/832384K available (15420K kernel code, 1216K rwdata, 5944K rodata, 3136K init, 1012K bss, 47104K reserved, 65536K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000]  Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 512 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: no VLPI support, no direct LPI support
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[    0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0
[    0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[    0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[    0.008842] Console: colour dummy device 80x25
[    0.013032] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[    0.023204] pid_max: default: 32768 minimum: 301
[    0.027892] LSM: Security Framework initializing
[    0.032469] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.039801] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.071710] ASID allocator initialised with 32768 entries
[    0.084805] rcu: Hierarchical SRCU implementation.
[    0.099557] EFI services will not be available.
[    0.111792] smp: Bringing up secondary CPUs ...
[    0.148417] Detected VIPT I-cache on CPU1
[    0.148449] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[    0.148488] CPU1: Booted secondary processor 0x0000000001 [0x410fd042]
[    0.148580] smp: Brought up 1 node, 2 CPUs
[    0.169718] SMP: Total of 2 processors activated.
[    0.174403] CPU features: detected: 32-bit EL0 Support
[    0.179541] CPU features: detected: CRC32 instructions
[    0.191291] CPU: All CPU(s) started at EL2
[    0.195072] alternatives: patching kernel code
[    0.200654] devtmpfs: initialized
[    0.218617] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.228060] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.237032] pinctrl core: initialized pinctrl subsystem
[    0.243082] DMI not present or invalid.
[    0.246922] NET: Registered protocol family 16
[    0.263659] DMA: preallocated 256 KiB pool for atomic allocations
[    0.269465] audit: initializing netlink subsys (disabled)
[    0.275067] audit: type=2000 audit(0.220:1): state=initialized audit_enabled=0 res=1
[    0.282572] cpuidle: using governor menu
[    0.287332] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.295636] Serial: AMBA PL011 UART driver
[    0.299483] imx mu driver is registered.
[    0.303315] imx rpmsg driver is registered.
[    0.361927] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.368310] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.374986] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.381673] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.390417] cryptd: max_cpu_qlen set to 1000
[    0.401825] ACPI: Interpreter disabled.
[    0.407905] iommu: Default domain type: Translated
[    0.412972] vgaarb: loaded
[    0.415690] SCSI subsystem initialized
[    0.419512] usbcore: registered new interface driver usbfs
[    0.424710] usbcore: registered new interface driver hub
[    0.430006] usbcore: registered new device driver usb
[    0.437165] mc: Linux media interface: v0.10
[    0.441140] videodev: Linux video capture interface: v2.00
[    0.446654] pps_core: LinuxPPS API ver. 1 registered
[    0.451524] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[    0.460657] PTP clock support registered
[    0.464920] EDAC MC: Ver: 3.0.0
[    0.469406] No BMan portals available!
[    0.473180] QMan: Allocated lookup table at (____ptrval____), entry count 65537
[    0.480847] No QMan portals available!
[    0.485279] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[    0.491984] FPGA manager framework
[    0.495637] Bluetooth: Core ver 2.22
[    0.498892] NET: Registered protocol family 31
[    0.503316] Bluetooth: HCI device and connection manager initialized
[    0.509660] Bluetooth: HCI socket layer initialized
[    0.514517] Bluetooth: L2CAP socket layer initialized
[    0.520808] imx-scu scu: NXP i.MX SCU Initialized
[    0.530686] random: fast init done
[    0.565611] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[    0.575131] imx8qxp-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[    0.583669] clocksource: Switched to clocksource arch_sys_counter
[    0.589657] VFS: Disk quotas dquot_6.6.0
[    0.593398] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.600959] pnp: PnP ACPI: disabled
[    0.634349] thermal_sys: Registered thermal governor 'step_wise'
[    0.634355] thermal_sys: Registered thermal governor 'power_allocator'
[    0.640577] NET: Registered protocol family 2
[    0.651511] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[    0.659567] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.667324] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)
[    0.674588] TCP: Hash tables configured (established 8192 bind 8192)
[    0.680899] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.687441] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.694579] NET: Registered protocol family 1
[    0.699242] RPC: Registered named UNIX socket transport module.
[    0.704831] RPC: Registered udp transport module.
[    0.709513] RPC: Registered tcp transport module.
[    0.714207] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.721071] PCI: CLS 0 bytes, default 64
[    0.725402] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    0.733933] kvm [1]: IPA Size Limit: 40bits
[    0.738495] kvm [1]: GICv3: no GICV resource entry
[    0.742945] kvm [1]: disabling GICv2 emulation
[    0.747392] kvm [1]: GIC system register CPU interface enabled
[    0.753251] kvm [1]: vgic interrupt IRQ1
[    0.757195] kvm [1]: Hyp mode initialized successfully
[    0.769219] Initialise system trusted keyrings
[    0.773512] workingset: timestamp_bits=44 max_order=18 bucket_order=0
[    0.788060] NFS: Registering the id_resolver key type
[    0.792839] Key type id_resolver registered
[    0.796947] Key type id_legacy registered
[    0.800950] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.807835] 9p: Installing v9fs 9p2000 file system support
[    0.829834] Key type asymmetric registered
[    0.833604] Asymmetric key parser 'x509' registered
[    0.838504] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.845851] io scheduler mq-deadline registered
[    0.850358] io scheduler kyber registered
[    0.872509] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[    0.883007] EINJ: ACPI disabled.
[    0.966938] mxs-dma 5b810000.dma-apbh: initialized
[    0.974599] Bus freq driver module loaded
[    0.987165] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.998538] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 57, base_baud = 5000000) is a FSL_LPUAR[    1.007725] printk: console [ttyLP0] enabled
[    1.007725] printk: console [ttyLP0] enabled
[    1.016128] printk: bootconsole [lpuart32] disabled
[    1.016128] printk: bootconsole [lpuart32] disabled
[    1.026236] fsl-lpuart 5a060000.serial: DMA tx channel request failed, operating without tx DMA
[    1.034993] fsl-lpuart 5a060000.serial: DMA rx channel request failed, operating without rx DMA
[    1.044156] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 58, base_baud = 5000000) is a FSL_LPUART
[    1.054476] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 59, base_baud = 5000000) is a FSL_LPUART
[    1.064761] 5a090000.serial: ttyLP3 at MMIO 0x5a090010 (irq = 60, base_baud = 5000000) is a FSL_LPUART
[    1.114850] imx-drm display-subsystem: parent device of /bus@56220000/ldb@562410e0/lvds-channel@0 is not available
[    1.137862] panel-simple lvds0_panel: lvds0_panel supply power not found, using dummy regulator
[    1.146824] panel-simple lvds1_panel: lvds1_panel supply power not found, using dummy regulator
[    1.164694] loop: module loaded
[    1.172979] imx ahci driver is registered.
[    1.186978] libphy: Fixed MDIO Bus: probed
[    1.192104] tun: Universal TUN/TAP device driver, 1.6
[    1.199533] thunder_xcv, ver 1.0
[    1.202822] thunder_bgx, ver 1.0
[    1.206099] nicpf, ver 1.0
[    1.212344] Freescale FM module, FMD API version 21.1.0
[    1.218454] Freescale FM Ports module
[    1.222128] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[    1.228219] fsl_dpa: FSL DPAA Ethernet driver
[    1.232933] fsl_advanced: FSL DPAA Advanced drivers:
[    1.237913] fsl_proxy: FSL DPAA Proxy initialization driver
[    1.243867] fsl_oh: FSL FMan Offline Parsing port driver
[    1.251604] hclge is initializing
[    1.254941] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[    1.262175] hns3: Copyright (c) 2017 Huawei Corporation.
[    1.267571] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[    1.274672] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    1.280477] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[    1.286321] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    1.292291] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[    1.299263] igb: Copyright (c) 2007-2014 Intel Corporation.
[    1.304896] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[    1.312735] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    1.319146] sky2: driver version 1.30
[    1.325439] VFIO - User Level meta-driver version: 0.3
[    1.335928] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.342484] ehci-pci: EHCI PCI platform driver
[    1.346996] ehci-platform: EHCI generic platform driver
[    1.352799] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[    1.359018] ohci-pci: OHCI PCI platform driver
[    1.363524] ohci-platform: OHCI generic platform driver
[    1.370626] usbcore: registered new interface driver usb-storage
[    1.385040] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[    1.395081] i2c /dev entries driver
[    1.413510] sdhci: Secure Digital Host Controller Interface driver
[    1.419753] sdhci: Copyright(c) Pierre Ossman
[    1.424711] Synopsys Designware Multimedia Card Interface Driver
[    1.432735] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.440513] mmc0: CQHCI version 5.10
[    1.476085] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[    1.489066] ledtrig-cpu: registered to indicate activity on CPUs
[    1.497365] usbcore: registered new interface driver usbhid
[    1.503034] usbhid: USB HID core driver
[    1.511058] No fsl,qman node
[    1.514041] Freescale USDPAA process driver
[    1.518242] fsl-usdpaa: no region found
[    1.522084] Freescale USDPAA process IRQ driver
[    1.539934] Galcore version 6.4.0.234062
[    1.567983] mmc0: Command Queue Engine enabled
[    1.572477] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[    1.583543] mmcblk0: mmc0:0001 8GUF4R 7.28 GiB
[    1.588249] mmcblk0boot0: mmc0:0001 8GUF4R partition 1 31.9 MiB
[    1.594307] mmcblk0boot1: mmc0:0001 8GUF4R partition 2 31.9 MiB
[    1.600418] mmcblk0rpmb: mmc0:0001 8GUF4R partition 3 4.00 MiB, chardev (237:0)
[    1.612810]  mmcblk0: p1 p2 p3 p4
[    1.620780] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    1.628733] NET: Registered protocol family 26
[    1.633924] NET: Registered protocol family 10
[    1.639180] Segment Routing with IPv6
[    1.642928] NET: Registered protocol family 17
[    1.647430] 8021q: 802.1Q VLAN Support v1.8
[    1.651675] lib80211: common routines for IEEE802.11 drivers
[    1.657473] 9pnet: Installing 9P2000 support
[    1.661806] tsn generic netlink module v1 init...
[    1.666590] Key type dns_resolver registered
[    1.671353] registered taskstats version 1
[    1.675480] Loading compiled-in X.509 certificates
[    1.705859] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[    1.730957] usb_phy_generic bus@5b000000:usb3-phy: bus@5b000000:usb3-phy supply vcc not found, using dummy regulator
[    1.743829] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[    1.758966] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.765621] [drm] No driver support for vblank timestamp query.
[    1.771626] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[    1.780131] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[    1.787714] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[    1.795311] imx-drm display-subsystem: failed to bind bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops): -517
[    1.805303] imx-drm display-subsystem: master bind failed: -517
[    1.811469] dpu-core 56180000.dpu: driver probed
[    1.816638] panel-simple lvds0_panel: lvds0_panel supply power not found, using dummy regulator
[    1.996118] pps pps0: new PPS source ptp0
[    2.008224] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    2.015074] fec 5b040000.ethernet: Using random MAC address: d2:56:64:b6:81:6d
[    2.023356] libphy: fec_enet_mii_bus: probed
[    2.029482] fec 5b040000.ethernet eth0: registered PHC device 0
[    2.110436] imx-rpmsg 90000000.rpmsg: assigned reserved memory node vdevbuffer
[    2.139732] virtio_rpmsg_bus virtio0: rpmsg host is online
[    2.167701] virtio_rpmsg_bus virtio1: rpmsg host is online
[    2.176482] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    2.183166] [drm] No driver support for vblank timestamp query.
[    2.189196] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[    2.197532] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[    2.204979] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[    2.213222] imx-drm display-subsystem: bound bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops)
[    2.222216] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
[    2.478400] Console: switching to colour frame buffer device 160x40
[    2.504293] imx-drm display-subsystem: fb0: imx-drmdrmfb frame buffer device
[    2.518210] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[    2.525948] debugfs: Directory 'mipi1-i2c1' with parent 'pm_genpd' already present!
[    2.533628] debugfs: Directory 'mipi1-i2c0' with parent 'pm_genpd' already present!
[    2.541327] debugfs: Directory 'mipi1-pwm0' with parent 'pm_genpd' already present!
[    2.548998] debugfs: Directory 'mipi1' with parent 'pm_genpd' already present!
[    2.565242] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    2.574960] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    2.581618] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    2.590258] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[    2.606524] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
[    2.702040] EXT4-fs (mmcblk0p2): 1 orphan inode deleted
[    2.707332] EXT4-fs (mmcblk0p2): recovery complete
[    2.715236] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.723438] VFS: Mounted root (ext3 filesystem) on device 179:2.
[    2.729551] devtmpfs: mounted
[    2.733642] Freeing unused kernel memory: 3136K
[    2.738279] Run /sbin/init as init process
init started: BusyBox v1.31.0 (2021-06-09 06:12:44 UTC)
starting pid 228, tty '': '/bin/mount -t proc proc /proc'
starting pid 229, tty '': '/bin/mount -t sysfs sysfs /sys'
starting pid 230, tty '': '/bin/mount -t devtmpfs devtmpfs /dev'
mount: /dev: devtmpfs already mounted on /dev.
starting p[    2.789501] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
id 231, tty '': '/bin/mount -o remount,rw /'
starting pid 232, tty '': '/bin/mkdir -p /dev/pts'
starting pid 233, tty '': '/bin/mount -t devpts devpts /dev/pts'
starting pid 234, tty '': '/bin/mount -a'
starting pid 235, tty '': '/etc/init.d/rcS'
Starting udev
[    2.939642] udevd[254]: starting version 3.2.8
[    2.946464] random: udevd: uninitialized urandom read (16 bytes read)
[    2.953360] random: udevd: uninitialized urandom read (16 bytes read)
[    2.959873] random: udevd: uninitialized urandom read (16 bytes read)
[    2.983486] udevd[255]: starting eudev-3.2.8
[    3.125141] [VPU Encoder] enable mu for core[0]
[    3.138065] [VPU Encoder] vpu encoder core[0] firmware version is 1.2.7
[    3.787314] EXT4-fs (mmcblk0p3): mounting ext3 file system using the ext4 subsystem
[    3.840313] EXT4-fs (mmcblk0p4): recovery complete
[    3.845721] EXT4-fs (mmcblk0p3): recovery complete
[    3.846056] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)
[    3.858698] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[    3.868678] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
/etc/rcS.d/S38dmesg.sh: line 17: /var/log: Is a directory
Starting vsftpd: OK
Starting system message bus: [    4.061511] urandom_read: 3 callbacks suppressed
dbus.
[    4.061519] random: dbus-daemon: uninitialized urandom read (12 bytes read)
[    4.070570] random: dbus-daemon: uninitialized urandom read (12 bytes read)
Starting Connection Manager
Configuring network interfaces... [    4.173284] random: connmand: uninitialized urandom read (8 bytes read)
[    4.225538] ybx ,ret=0
[    4.228821] RTL9000AA/AN Ethernet 5b040000.ethernet-1:00: attached PHY driver [RTL9000AA/AN Ethernet] (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
RTNETLINK answers: File exists
Running local boot scripts (/etc/rc.local).
/etc/rc5.d/S10rc.local: line 38: /home/root/watchdog_open: No such file or directory
[    4.415028] module inint ~~~~~~~~~~
run /vendor/cr/sh/crboot.sh
Starting Dropbear SSH server: rm: cannot remove '/usbpic': No such file or directory
-------------------------the num=2563-----------------
dropbear.
/home/root/isvalidip.sh: line 29: crsetprop: command not found
Starting rpcbind daemon...done.
starting statd: done
Starting atd: OK
exportfs: can't open /etc/exports for reading
NFS daemon support not enabled in kernel
Starting Telephony daemon
Starting Linux NFC daemon
Starting crond: OK
starting pid 590, tty '/dev/ttyLP0': '/sbin/getterror, map_prop_area failed, shmget()=-1
could not set property error:-3
could not set property
run /vendor/cr/bin/crinit
version:1.0.2.210914, /vendor/cr/bin/crinit
file open error
shaderPath [glowLine] Program OK
shaderPath [light] Program OK
shaderPath [roundBrushLine] Program OK
shaderPath [pointFont] Program OK
shaderPath [texture] Program OK
shaderPath [textureFont] Program OK
shaderPath [textureFrameAct] Program OK
logtotal size is out range
/log/cr/19700101_00000167.log is out ot date
[   17.461142] random: crng init done
[   17.464562] random: 1 urandom warning(s) missed due to ratelimiting
[   33.863737] usb_otg1_vbus: disabling
[   33.867382] SD1_SPWR: disabling

imx8qxpc0mek login:
imx8qxpc0mek login: root

ls
eee
[ 5206.513026] ci_hdrc ci_hdrc.0: remove, state 1
[ 5206.518249] usb usb1: USB disconnect, device number 1
[ 5206.524029] usb 1-1: USB disconnect, device number 2
[ 5206.582439] ci_hdrc ci_hdrc.0: USB bus 1 deregistered
[ 5211.599714] ci_hdrc ci_hdrc.0: timeout waiting for 00000800 in OTGSC

 

 

 

 

0 件の賞賛
返信
0 返答(返信)