IMX8QXP SCFW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP SCFW

1,945 Views
gravity_one
Contributor III

hello,

version: imx-scfw-porting-kit-1.7.0

i want to see SCFW console log, set :

make qx R=B0 B=mek M=1 D=1 U=1 V=1

 

but SCFW print :
>$
Hello from SCU (Build 5126, Commit 0d54291f, Dec 17 2020 03:06:47)

SCFW: DDR frequency = 1200000000
ROM boot time = 59240 usec
Boot time = 28261 usec
Banner = 9 usec
Init = 8656 usec
Config = 2586 usec
DDR = 11123 usec
SConfig = 273 usec
Prep = 3363 usec

Incorrect SECO FW version 2.5.4 (3.7.4 or later required)

*** Debug Monitor ***

>$

 

 

 

0 Kudos
Reply
1 Reply

1,941 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gravity

 

all versions of software components (like SCFW, SECO e.t.c.) should be aligned

according to Release Notes document for each BSP. Not recommneded to mix them with

other versions:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

1.jpg

 

 

Best regards
igor

0 Kudos
Reply