IMX8QXP Ethernet strap options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP Ethernet strap options

2,976 Views
Chethanbg
Contributor III

Hi,

As per IMX8QXP eval board there is mode2[3:0] settings strap resistors options

In our custom board we are using IMX8QXP with KSZ8041RNL in RMII (10/100Mbps )

My query is

In eval board these strap resistors are belongs to AR8031 or IMX8QXP?

We are using IMX8QXP with KSZ8041 so any mode settings to be done through hardware to select RMII?

In Datasheet or Reference manual of IMX8QXP there is no information on MODE setting strap resistors

Kindly clarify

0 Kudos
Reply
3 Replies

2,947 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Chethanbg,

I hope you are doing well.

In i.MX8QXP EVK, the strap resistors belong to the Ethernet PHY chip AR8031 and are configured as per the modes mentioned in the Ethernet PHY datasheet.

So, one can refer to the KSZ8041 datasheet and can configure the strap resistors accordingly in your custom board.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

2,941 Views
Chethanbg
Contributor III

Dear @riteshmpatel 

Thanks for the reply.Currently in RMII mode we are using 25 Mhz crystal mode

The KSZ8041RNL generates the 50MHz RMII REF_CLK and outputs it to the MAC

attached is the block diagram for your reference.

In pin configuration RGMII_TXC should be configured as ENET0_RCLK50M_IN input  right?

IMX8QXP_ENET0_RGMII_TXC_CONN_ENET0_RCLK50M_IN                               0x06000061

 

Also let us know the pad settings  0x06000061 is correct

0 Kudos
Reply

2,938 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Chethanbg,

I request you to please raise a new ticket for the additional questions.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply