IMX8QX DDR3L/DDR3 application design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QX DDR3L/DDR3 application design

742件の閲覧回数
alexjiang
Contributor II

Hi,

    Our design platform :IMX8QX : MIMX8QX6AVLFZAC  +  16bit DDR3L/DDR3.

    IMX8QX support 32bit+8bit DDR3L. But we need only 1pcs 16bit DDR3L. 

1. Can we design with only 1 pcs 16bit DDR3L(lower 16 bit), and leave 16~40bit DQ floating?

2. Whether IMX8QX support DDR3 voltage level: 1.5V?

0 件の賞賛
返信
3 返答(返信)

733件の閲覧回数
KalaimaniArumugamdev
Contributor III

Hi @alexjiang 

Q1: Can we design with only 1 pcs 16bit DDR3L(lower 16-bit), and leave 16~40bit DQ floating?

Ans: Yes, You can use 16bit addressing and leave 16~40bit DQ as a float. Because MMDC is a multi-mode DDR controller that supports DDR3/DDR3L at 16bit mode.

Q2:Whether IMX8QX support DDR3 voltage level: 1.5V?

Ans: Yes, Refer to datasheet page number 13.Screenshot 2023-01-16 9.53.27 AM.png

 

0 件の賞賛
返信

717件の閲覧回数
alexjiang
Contributor II

Hi,

 @KalaimaniArumugamdev 

Q2:Whether IMX8QX support DDR3 voltage level: 1.5V?

InkedScreenshot 2023-01-16 9.53.27 AM.jpg

the picture show IMX8QX VDD/VDDQ  I/O  support DDR3L:1.35V, MAX  DDR3L voltage :1.45V. 

and IMX8QX datasheet does not show whether support  DDR3: 1.5V, 1.425~1.57V(DDR3 voltage range),

only show DDR PHY supplies  VDD_DDR_VDDQ max:1.75V.  Does it means that we can use DDR3 IC and supply 1.5V voltage to VDD/VDDQ?  

 

 
0 件の賞賛
返信

710件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @alexjiang,

i.MX8QXP supports DDR3L and LPDDR4 only.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信