IMX8QM single mode LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM single mode LVDS

1,606 Views
linjermmy
Contributor I

Hi NXP experts,

Could you please help me configure the LVDS to single mode ?

I modify fsl-imx8qxp-mek-jdi-wuxga-lvds0-panel.dts to single mode lvds but the result is not positive.

The resolution is 1280x480@60.

Is there single mode example ?

BR.

Jush

0 Kudos
Reply
3 Replies

1,532 Views
linjermmy
Contributor I

Hi NXP experts,

Is there any update?

0 Kudos
Reply

1,532 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jush,

The default fsl-imx8qxp-mek-jdi-wuxga-lvds0-panel.dtb: Supports the dual channel LVDS panel, connecting the two mini-SAS ports with the LVDS0 CH0 and LVDS0 CH1. What have you modified? Here could you tell us which screen you are using? What's

Have a nice day

Best Regards

Rita

0 Kudos
Reply

1,532 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 Kudos
Reply