IMX8QM bring up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8QM bring up

1,151 次查看
Vishnu13
Contributor I

Hi,

I have encountered an error while bringing up IMX8QM MEK using serial boot and uuu.

I have followed the instructions for the hardware setup including the switch configuration (001000).

uuu version : 1.4.243

Image zip file : LF_v5.15.71-2.2.0_images_IMX8QMMEK.zip

Error log:

=======================================================================

quest@TVMLT0815:~/Downloads$ sudo ./uuu LF_v5.15.71-2.2.0_images_IMX8QMMEK.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Wait for Known USB Device Appear...
Error: fail open file: >LF_v5.15.71-2.2.0_images_IMX8QMMEK.zip/uuu.auto

======================================================================

 

 

0 项奖励
回复
1 回复

1,114 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Vishnu13 

According to the error message: 

You might need to check the permission for these files needed to be executed in the current directory.

And if uuu.auto is existing in the correct directory for execution.

 

Best regards

Harvey

0 项奖励
回复