IMX8QM(MAX) CUSTOM HARDWARE DESIGN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM(MAX) CUSTOM HARDWARE DESIGN

4,159 Views
peteramond
Contributor V

Hi All,

I'm trying to design a custom hardware design based on MIMX8QM5AVUFFAB (IMX8QM) processor. I'm referring to i.MX 8QuadMax Multisensory Enablement Kit (MEK) development board >> Link <<

When I was doing custom hardware design for IMAX6Q processor I had all the following documents. (Attached)

  • i.MX 6Dual/6Quad Applications Processor Reference Manual
  • Hardware Development Guide for i.MX 6QuadPlus, 6Quad
  • i.MX 6Dual/6Quad Power Consumption Measurement

1) But I couldn't find any document for IMX8QM processor. Could you please provide me all those documents. It's really helpful to have memory layout routing rules and etc as well. 

2) As well as can I have design files and layout files which can open in Altium for i.MX 8QuadMax Multisensory Enablement Kit (MEK) development board.

3) For DDR calibration what kind of tool are you using ? The same tool as IMAX6Q stressapp tester ?

4) If the design files and layout files which can open in Altium for i.MX 8QuadMax Multisensory Enablement Kit (MEK) development board is not available; can I have design files for MCIMX8M-EVK: Evaluation Kit for the i.MX 8M Applications Processor >> Link <<

Regards,

Peter.

4 Replies

3,891 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

one can look at

i.MX 8 Family Applications Processor | Arm Cortex-A53/A72/M4 | NXP 

i.MX 8QuadMax/i.MX 8QuadXPlus Hardware Developer’s Guide

i.MX8 MEK Base Board Design Files

Schematic for MCIMX8QM-CPU

Layout for MCIMX8QM-CPU

Other documents and tools can be obtained through local nxp marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,891 Views
peteramond
Contributor V

igorpadykov

Thank you for your reply.

The layout files you have shared is only the base board.

pastedImage_1.png

But I need to look into processor board layout files to do my custom hardware design. I must be thankful to you if you can share layout files of the following board (which can open in Altium designer) . 

pastedImage_2.png

Regards,

Peter.

0 Kudos
Reply

3,891 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

unfortunately altium formats are not supported by nxp. For other documents please apply

to local office.

Best regards
igor

3,891 Views
peteramond
Contributor V

igorpadykov

It's not a problem whether it's Altium or any other design software. I can import it anyway. Could you please share the layout design files of following processor board. In your first comment you just shared base board layout. I need following board layout files in any format.

pastedImage_1.png

Regards,

Peter.

0 Kudos
Reply