IMX8MQ: compatible LPDDR4 devices?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MQ: compatible LPDDR4 devices?

1,226件の閲覧回数
N_Coesel
Contributor III

Hello,

I'm running into trouble finding Micron memory for an IMX8MQ design. I have used the same part ( MT53E768M32D4DT-053 WT:E ) which is on the IMX8MQ EVK board but this isn't available anywhere. The same goes for any LPDDR device from Micron with a similar capacity (2GB to 4GB; I don't care right now). Are there any alternatives out there which are available?

thanks in advance!

0 件の賞賛
返信
1 返信

1,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nico

file was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信