IMX8MP on android 11 Bluetooth HFP SOC audio output problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP on android 11 Bluetooth HFP SOC audio output problem

1,419件の閲覧回数
Wiser-Kuo
Contributor I

We use BCM4375 bluetooth (ap6275 chipset)  on IMX8MP Android 11,  and modified BT HAL to hardware/broadcom/libbt to make it work.

BT A2DP transmission works fine. (headphone without mic) , in/out BT audio transmit without problem.

 

BT SCO  HFP : (headset with microphone)

While IMX8MP-AP6275 connected to a headset  and use ZOOM app to make call with  ZOOM software on PC ,

Audio output from headset has lot of noise (data transmit from PC)  , it sounds like under-sampled and very low frequency sound.

My headset is not support WBS ,  so SCO rate is set at 8K , instead of 16k while running HFP.

I've tried to  resample rates in tinyalsa_hal.cpp but it's not work.

( create_resampler with 8k in start_output_stream while AUDIO_DEVICE_OUT_ALL_SCO)

 

Is audo & BT HAL of iMX8mp support HFP while WBS disabled? 

Is there any patches to make it works properly?

 

Attachment are modified patches for disable WBS and add SCO interface. 

  

螢幕擷取畫面 2022-09-15 154104.jpg

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)