IMX8MP compilation with toolchain - general question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP compilation with toolchain - general question

1,003 Views
jake4
Contributor III

What are the pros and cons of using the generic toolchain for IMX8MP, and NXP specific toolchain. 

like the arm gnu toolchain versus the toolchain given by NXP aka built using yocto or debian flex environment. ( say fsl-linux-wayland) 

Is the toolchain custom built for NXP are optimized for the CPU?

0 Kudos
Reply
1 Reply

977 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @jake4,

Thank you for contacting NXP Support!

 

Generic ARM GNU Toolchain
Pros:

Portability: Works across multiple ARM platforms, not tied to NXP-specific BSP.
Community Support: Large user base, frequent updates, and well documented.
Ease of Setup: Simple installation from official ARM releases or package managers.
Flexibility: Ideal for bare metal or minimal Linux environments without vendor dependencies.

Cons:

No BSP Integration: Does not include NXP specific patches or optimizations for i.MX hardware.
Limited Hardware Acceleration Support: May lack tuned libraries for GPU/VPU, DSP, or NEON optimizations.
Potential ABI Differences: Could lead to incompatibilities with prebuilt NXP binaries or SDK components.


NXP-Specific Toolchain (Yocto SDK)
Pros:

Optimized for i.MX SoCs: Includes patches and compiler flags tuned for Cortex A53 (i.MX8MP) and integrated accelerators.
Full BSP Integration: Matches kernel, U-Boot, and libraries provided by NXP.
Multimedia and Security Support: Ensures compatibility with NXP’s GPU/VPU drivers, secure boot, and hardware crypto.
Long Term Support: Maintained alongside NXP’s LTS releases for Yocto and Debian.

Cons:

Less Portable: Tied to NXP BSP; harder to reuse for non NXP platforms.
Complex Setup: Requires Yocto build or Flex environment, which can be time consuming.
Version Lock In: Updates depend on NXP release cycles, not upstream GCC.

Best Regards,
Chavira