IMX8MP and accellerated jpeg decoder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP and accellerated jpeg decoder

1,819件の閲覧回数
stefanop
Contributor I

Hi,

I'm working with and IMX8MP I need to decompress a motion jpeg video stream.

I'm using Yocto gatesgarth and the libimxvpuapi2 version v2.1.0.

To test the decoder I tried to launch the code example jpeg-dec-example contained in the libimxvpuapi2 but i recevied the followoing error

OMX JPEG ! HantroHwDecOmx_decoder_create_jpeg JpegDecInit error openmax_il/source/decoder/codec_jpeg.c:1045
../git/imxvpuapi2/imxvpuapi2_imx8m_hantro_decoder.c:1372 (imx_vpu_api_dec_open)   ERROR: could not create codec
../git/imxvpuapi2/imxvpuapi2_jpeg.c:200 (imx_vpu_api_jpeg_dec_open)   ERROR: could not open JPEG decoder: error
could not open VPU JPEG decoder
../git/imxvpuapi2/imxvpuapi2_imx8m_hantro_decoder.c:1410 (imx_vpu_api_dec_close)   debug: closing decoder
Segmentation fault

 

My question is: The VPU of the IMX8MP processor is able to do an hardware accelerated decoding of jpeg images?

 Thanks in advance.

0 件の賞賛
返信
3 返答(返信)

1,809件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello stefanop, you can use the same vpu encode api as mpeg4/h.264 to encode mjpeg, just set different format.

mxc_vpu_test is open source, suppose you can get the source from our formal release.

The only work you need to do is adjust the memory pool to allow large memory allocation and set proper value for 'VPU_ENC_BITS_BUF_SIZE' accordingly just like mentioned above.

For the libimxvpuapi, it was developed by third-party, you can ask help in this community

or you can get NXP formal release package from BSP  NXP offical site.

 

Regards

0 件の賞賛
返信

1,803件の閲覧回数
stefanop
Contributor I

Thanks for your reply,  only one more clarification:

I see your speaking about encode functions but I need to decode an mjpeg stream.

It is possible to use the same VPU APIs used for decoding mpeg4/h.264 to decode also a jpeg image?

Thanks

 

 

0 件の賞賛
返信

1,769件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes it can be used.

0 件の賞賛
返信