IMX8MP NPU produce same output with same input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP NPU produce same output with same input

2,078 Views
RIMASTA
Contributor I

IMX8MP produce same output with same input. Same as

tensorflow-imx at branch lf-5.10.52_2.1.0, 
Dynamic link to:
libusb-1.0.so.0
libtensorflow-lite.so.2.9.1
libopencv_core.so.406
libopencv_video.so.406
libopencv.....
Gstreamer is from NXP yocto build, Initializing GStreamer Core Library version 1.20.3
 
in words:
Here are use cases.

Case 1:
  1. I open camera using LIBUSB, and then close it (I do not read anything just, claim and unclaim interface).
  2. I open camera with opencv gstreamer backend, after NPU initialization -> I get the same output with different input from NPU.
Case 2:
   1.I DO NOT open+close with LIBUSB.
   2.I open camera with opencv gstreamer backend after NPU initialization -> WORKS!
 
Case 3:
  1. I open camera using LIBUSB, and then close it (I do not read anything, just claim and unclaim interface).
  2. I open camera with opencv V4l2 backend after NPU initialization -> WORKS!
Questions:
  • How can opencv+gstreamer change output from NPU, I only use cpu plugins in gst?
  • Can you review the off init() USBCameraDevice?
  • Can you review off initialization off NPU, or provide a working example?

Same bug is reported here:
 
 

With some differences:
I use C++ and vxdelegate.

I cannot reproduce his result, I must do the LIBUSB init().

Code:


bool init()
{
if (libusb_init(&context_) != 0)
{
std::cout << "libusb_init failed " << std::endl;
return false;
}

handle_ = libusb_open_device_with_vid_pid(context_, 0x0BDA, 0x5880);
if (handle_ == nullptr)
{
std::cout << "libusb_open_device_with_vid_pid failed " << std::endl;
return false;
}
kernel_driver_attached_ = (libusb_kernel_driver_active(handle_, 0) == 1);
if (kernel_driver_attached_)
{
if (libusb_detach_kernel_driver(handle_, 0) != 0)
{
std::cout << "libusb_detach_kernel_driver failed " << std::endl;
return false;
}
}
if (libusb_claim_interface(handle_, 0) != 0)
{
std::cout << "libusb_claim_interface " << std::endl;
return false;
}
init_ok_ = true;
return true;
}

 

#include "bug.h"
#include "tensorflow/lite/delegates/external/external_delegate.h"
#include "tensorflow/lite/interpreter.h"
#include "tensorflow/lite/kernels/register.h"
#include "tensorflow/lite/model.h"
#include "tensorflow/lite/optional_debug_tools.h"
#include "tensorflow/lite/tools/delegates/delegate_provider.h"
#include "USB_camera_device.hpp"
#include <chrono>
#include <ctime>
#include <iostream>
#include <numeric>

CameraNode::CameraNode() : running_(false)
{
USBCameraDevice camera_interface;
bool camera_interface_ok = camera_interface.init(); // comment this no bug!
}

CameraNode::~CameraNode()
{
running_ = false;
}

void CameraNode::start()
{
running_ = true;
std::thread t1(&CameraNode::captureThread, this);
std::thread t2(&CameraNode::processingThread, this);
t1.join();
t2.join();
}

void CameraNode::captureThread()
{
auto gstreamerPipeline =
"v4l2src device=/dev/videoFRONT ! video/x-raw,format=YUY2,width=812,height=420,framerate=25/1 ! appsink";
std::this_thread::sleep_for(std::chrono::milliseconds(20000));

std::cout << "cam open " << std::endl;
// cv::VideoCapture cap("/dev/videoFRONT", cv::CAP_V4L2); // CAP_V4L2 no bug, bug with gstreamer!

// if (!cap.isOpened())
// {
// std::cerr << "Error: Unable to open camera at" << std::endl;
// return;
// }

// // Set camera properties (optional, but recommended)
// // Set the desired properties for YUY2 format
// cap.set(cv::CAP_PROP_FRAME_WIDTH, 812);
// cap.set(cv::CAP_PROP_FRAME_HEIGHT, 420);
// cap.set(cv::CAP_PROP_FPS, 25);
// cap.set(cv::CAP_PROP_FOURCC, cv::VideoWriter::fourcc('Y', 'U', 'Y', 'V')); // YUY2 format
// cap.set(cv::CAP_PROP_CONVERT_RGB, 0);

cv::VideoCapture cap;
cap.open(gstreamerPipeline, cv::CAP_GSTREAMER); // <- bug
std::cout << "done open " << std::endl;

if (!cap.isOpened())
{
std::cerr << "Error: Unable to open the camera using GStreamer pipeline." << std::endl;
running_ = false;
return;
}
std::cout << "Camera opened successfully." << std::endl;

cv::Mat frame;
while (running_)
{
cap >> frame;
std::cout << "cap cnls: " << frame.channels() << " w " << frame.cols << " " << frame.rows << std::endl;

if (frame.empty())
{
std::cerr << "Error: Received empty frame." << std::endl;
running_ = false;
break;
}
}
cap.release();
}

void CameraNode::processingThread()
{
// #################REVIEW START#############################
std::unique_ptr<tflite::Interpreter> npu_interpreter_cpu_fallback;
std::string model_path_ =
"/usr/share/camera/models/seg_14x14_752_192.tflite"; // ANY MODEL FAILS INCLUDING MOBILENET from tensorflow
// examples
std::unique_ptr<tflite::FlatBufferModel> model_ = tflite::FlatBufferModel::BuildFromFile(model_path_.c_str());
tflite::ops::builtin::BuiltinOpResolver resolver_;
tflite::InterpreterBuilder builder(*model_, resolver_);

builder(&npu_interpreter_cpu_fallback);
std::string delegate_string_ = "/usr/lib/libvx_delegate.so";

auto delegate_options_ = TfLiteExternalDelegateOptionsDefault(delegate_string_.c_str());
auto delegate_ptr_ = TfLiteExternalDelegateCreate(&delegate_options_);
auto ok = npu_interpreter_cpu_fallback->ModifyGraphWithDelegate(delegate_ptr_);
std::cout << "allocate " << std::endl;
if (npu_interpreter_cpu_fallback->AllocateTensors() != kTfLiteOk)
{
std::cout << "npu ok " << std::endl;
}
// #################REVIEW END#############################

while (running_)
{
auto in_tensor = npu_interpreter_cpu_fallback->input_tensor(0);
auto input_width = in_tensor->dims->data[2];
auto input_height = in_tensor->dims->data[1];
auto input_channels = 3;

cv::Mat randomImage(input_height, input_width, CV_8UC3);
cv::randu(randomImage, cv::Scalar(0, 0, 0), cv::Scalar(255, 255, 255));
int out_sum = 0;
int in_sum = 0;

// Retrieve the latest frame safely
memcpy(npu_interpreter_cpu_fallback->typed_input_tensor<uint8_t>(0),
randomImage.data,
input_width * input_height * input_channels * sizeof(uint8_t));

for (size_t i = 0; i < input_channels * input_width * input_height; i++)
{
in_sum += npu_interpreter_cpu_fallback->typed_input_tensor<uint8_t>(0)[i];
}
std::cout << "invoke, input sum " << in_sum << std::endl;
auto inference_ok = npu_interpreter_cpu_fallback->Invoke();

cv::Mat output;
// std::cout << " SIZE " << npu_interpreter_cpu_fallback->output_tensor(0)->dims->size << std::endl;

auto output_height_ = npu_interpreter_cpu_fallback->output_tensor(0)->dims->data[1];
int output_channels_ = 1;
auto output_width_ = 1;

if (npu_interpreter_cpu_fallback->output_tensor(0)->dims->size > 2)
{
auto output_width_ = npu_interpreter_cpu_fallback->output_tensor(0)->dims->data[2];
output_channels_ = npu_interpreter_cpu_fallback->output_tensor(0)->dims->data[3];
}

output.create(output_height_, output_width_, CV_8UC(output_channels_));
switch (npu_interpreter_cpu_fallback->output_tensor(0)->type)
{
case kTfLiteUInt8:
{
int s = output_channels_ * output_height_ * output_width_;
memcpy(output.data,
npu_interpreter_cpu_fallback->typed_output_tensor<uint8_t>(0),
output_channels_ * output_height_ * output_width_ * sizeof(uint8_t));
for (size_t i = 0; i < s; i++)
{
out_sum += int(npu_interpreter_cpu_fallback->typed_output_tensor<uint8_t>(0)[i]);
}

break;
}
case kTfLiteInt8:
case kTfLiteFloat32:
case kTfLiteInt16:
case kTfLiteInt32:
case kTfLiteBool:
case kTfLiteNoType:
case kTfLiteFloat64:
case kTfLiteInt64:
case kTfLiteString:
case kTfLiteComplex64:
case kTfLiteComplex128:
case kTfLiteFloat16:
case kTfLiteUInt64:
case kTfLiteResource:
case kTfLiteVariant:
case kTfLiteUInt32:
case kTfLiteUInt16:
default:
{
break;
}
}

if (!output.empty())
{
std::cout << "Sum of pixels in the latest frame 2: " << out_sum << std::endl;
std::this_thread::sleep_for(std::chrono::milliseconds(2));
}
}
}

 

#ifndef CAMERANODE_H
#define CAMERANODE_H

#include <atomic>
#include <ctime>
#include <mutex>
#include <opencv2/opencv.hpp>
#include <thread>

class CameraNode
{
public:
CameraNode();
~CameraNode();

void start();

private:
void captureThread();
void processingThread();

std::atomic<bool> running_;
};

#endif // CAMERANODE_H

Log from gstreamer:

0:00:00.004675375 94448 0xffff781cfe00 INFO                GST_INIT gst.c:592:init_pre: Initializing GStreamer Core Library version 1.20.3
0:00:00.005013125 94448 0xffff781cfe00 INFO                GST_INIT gst.c:593:init_pre: Using library installed in /usr/lib
0:00:00.005216250 94448 0xffff781cfe00 INFO                GST_INIT gst.c:611:init_pre: Linux occulus93f0 5.15.52-5.15.87-2.2.0-greenworks+g8b2bcc215bd8+p10 #1 SMP PREEMPT Thu Feb 2 07:57:31 UTC 2023 aarch64
0:00:00.007921375 94448 0xffff781cfe00 INFO                GST_INIT gstmessage.c:129:_priv_gst_message_initialize: init messages
0:00:00.015012375 94448 0xffff781cfe00 INFO                GST_INIT gstcontext.c:86:_priv_gst_context_initialize: init contexts
0:00:00.016300250 94448 0xffff781cfe00 INFO      GST_PLUGIN_LOADING gstplugin.c:324:_priv_gst_plugin_initialize: registering 0 static plugins
0:00:00.016978250 94448 0xffff781cfe00 INFO      GST_PLUGIN_LOADING gstplugin.c:232:gst_plugin_register_static: registered static plugin "staticelements"
0:00:00.017076000 94448 0xffff781cfe00 INFO      GST_PLUGIN_LOADING gstplugin.c:234:gst_plugin_register_static: added static plugin "staticelements", result: 1
0:00:00.017446875 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistry.c:1827:ensure_current_registry: reading registry cache: /home/root/.cache/gstreamer-1.0/registry.aarch64.bin
Sum of pixels in the latest frame 2: 12241
0:00:00.065254875 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistrybinary.c:683:priv_gst_registry_binary_read_cache: loaded /home/root/.cache/gstreamer-1.0/registry.aarch64.bin in 0.047598 seconds
0:00:00.065506625 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistry.c:1693:scan_and_update_registry: Validating plugins from registry cache: /home/root/.cache/gstreamer-1.0/registry.aarch64.bin
invoke, input sum 55062968
0:00:00.079203875 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistry.c:1375:gst_registry_scan_path_level:<registry0> cached info for /usr/lib/gstreamer-1.0/libgstvideo4linux2.so is stale
Sum of pixels in the latest frame 2: 12251
0:00:00.000165000 94476 0xaaaacbe10400 INFO                GST_INIT gst.c:592:init_pre: Initializing GStreamer Core Library version 1.20.3
0:00:00.000265125 94476 0xaaaacbe10400 INFO                GST_INIT gst.c:593:init_pre: Using library installed in /usr/lib
0:00:00.000294125 94476 0xaaaacbe10400 INFO                GST_INIT gst.c:611:init_pre: Linux occulus93f0 5.15.52-5.15.87-2.2.0-greenworks+g8b2bcc215bd8+p10 #1 SMP PREEMPT Thu Feb 2 07:57:31 UTC 2023 aarch64
0:00:00.000782375 94476 0xaaaacbe10400 INFO                GST_INIT gstmessage.c:129:_priv_gst_message_initialize: init messages
0:00:00.002059375 94476 0xaaaacbe10400 INFO                GST_INIT gstcontext.c:86:_priv_gst_context_initialize: init contexts
0:00:00.002547375 94476 0xaaaacbe10400 INFO      GST_PLUGIN_LOADING gstplugin.c:324:_priv_gst_plugin_initialize: registering 0 static plugins
0:00:00.002815500 94476 0xaaaacbe10400 INFO      GST_PLUGIN_LOADING gstplugin.c:232:gst_plugin_register_static: registered static plugin "staticelements"
0:00:00.002855000 94476 0xaaaacbe10400 INFO      GST_PLUGIN_LOADING gstplugin.c:234:gst_plugin_register_static: added static plugin "staticelements", result: 1
0:00:00.002962000 94476 0xaaaacbe10400 INFO            GST_REGISTRY gstregistry.c:1862:ensure_current_registry: registry reading and updating done, result = 1
0:00:00.002991875 94476 0xaaaacbe10400 INFO                GST_INIT gst.c:833:init_post: GLib runtime version: 2.72.3
0:00:00.003016750 94476 0xaaaacbe10400 INFO                GST_INIT gst.c:835:init_post: GLib headers version: 2.72.3
0:00:00.003037250 94476 0xaaaacbe10400 INFO                GST_INIT gst.c:837:init_post: initialized GStreamer successfully
invoke, input sum 55069542
Sum of pixels in the latest frame 2: 12251
0:00:00.065827250 94476 0xaaaacbe10400 INFO      GST_PLUGIN_LOADING gstplugin.c:987:_priv_gst_plugin_load_file_for_registry: plugin "/usr/lib/gstreamer-1.0/libgstvideo4linux2.so" loaded
0:00:00.223206250 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistry.c:1794:scan_and_update_registry: Registry cache changed. Writing new registry cache
0:00:00.223331125 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistrybinary.c:431:priv_gst_registry_binary_write_cache: Building binary registry cache image
0:00:00.244991125 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistrybinary.c:463:priv_gst_registry_binary_write_cache: Writing binary registry cache
invoke, input sum 55112192
0:00:00.278634500 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistrybinary.c:314:gst_registry_binary_cache_finish: Wrote binary registry cache
0:00:00.278768250 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistry.c:1803:scan_and_update_registry: Registry cache written successfully
0:00:00.278894125 94448 0xffff781cfe00 INFO            GST_REGISTRY gstregistry.c:1862:ensure_current_registry: registry reading and updating done, result = 1
0:00:00.279017375 94448 0xffff781cfe00 INFO                GST_INIT gst.c:833:init_post: GLib runtime version: 2.72.3
0:00:00.279165625 94448 0xffff781cfe00 INFO                GST_INIT gst.c:835:init_post: GLib headers version: 2.72.3
0:00:00.279259125 94448 0xffff781cfe00 INFO                GST_INIT gst.c:837:init_post: initialized GStreamer successfully
0:00:00.280262125 94448 0xffff781cfe00 INFO            GST_PIPELINE gstparse.c:344:gst_parse_launch_full: parsing pipeline description 'v4l2src device=/dev/videoFRONT ! video/x-raw,format=YUY2,width=812,height=420,framerate=25/1 ! appsink'
Sum of pixels in the latest frame 2: 12251
invoke, input sum 55048696
0:00:00.333112125 94448 0xffff781cfe00 INFO      GST_PLUGIN_LOADING gstplugin.c:987:_priv_gst_plugin_load_file_for_registry: plugin "/usr/lib/gstreamer-1.0/libgstvideo4linux2.so" loaded
0:00:00.333303750 94448 0xffff781cfe00 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "v4l2src"
0:00:00.356930500 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseSrc@0xffff793ec160> adding pad 'src'
0:00:00.363878250 94448 0xffff781cfe00 INFO      GST_PLUGIN_LOADING gstplugin.c:987:_priv_gst_plugin_load_file_for_registry: plugin "/usr/lib/gstreamer-1.0/libgstapp.so" loaded
0:00:00.364000875 94448 0xffff781cfe00 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "appsink"
0:00:00.364985000 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseSink@0xffff62957c90> adding pad 'sink'
0:00:00.365291500 94448 0xffff781cfe00 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "pipeline"
0:00:00.366244500 94448 0xffff781cfe00 INFO            GST_PIPELINE gst/parse/grammar.y:683:gst_parse_perform_link: linking some pad of GstV4l2Src named v4l2src0 to some pad of GstAppSink named appsink0 (0/0) with caps "video/x-raw, format=(string)YUY2, width=(int)812, height=(int)420, framerate=(fraction)25/1"
Sum of pixels in the latest frame 2: 12251
0:00:00.376754500 94448 0xffff781cfe00 INFO      GST_PLUGIN_LOADING gstplugin.c:987:_priv_gst_plugin_load_file_for_registry: plugin "/usr/lib/gstreamer-1.0/libgstcoreelements.so" loaded
0:00:00.377027125 94448 0xffff781cfe00 INFO     GST_ELEMENT_FACTORY gstelementfactory.c:489:gst_element_factory_create_with_properties: creating element "capsfilter"
0:00:00.377737125 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseTransform@0xffff793fc100> adding pad 'sink'
0:00:00.377952000 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:759:gst_element_add_pad:<GstBaseTransform@0xffff793fc100> adding pad 'src'
0:00:00.378164875 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2069:gst_bin_get_state_func:<pipeline0> getting state
0:00:00.378436000 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to NULL
0:00:00.378571875 94448 0xffff781cfe00 INFO               GST_EVENT gstevent.c:1660:gst_event_new_reconfigure: creating reconfigure event
0:00:00.378761875 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstutils.c:1816:gst_element_link_pads_full: trying to link element v4l2src0:(any) to element capsfilter0:sink
0:00:00.378881375 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:1016:gst_element_get_static_pad: found pad capsfilter0:sink
0:00:00.379019375 94448 0xffff781cfe00 INFO                GST_PADS gstutils.c:1632:prepare_link_maybe_ghosting: v4l2src0 and capsfilter0 in same bin, no need for ghost pads
0:00:00.379178750 94448 0xffff781cfe00 INFO                GST_PADS gstpad.c:2382:gst_pad_link_prepare: trying to link v4l2src0:src and capsfilter0:sink
0:00:00.379337750 94448 0xffff781cfe00 INFO                GST_PADS gstpad.c:4357:gst_pad_peer_query:<capsfilter0:src> pad has no peer
0:00:00.379531625 94448 0xffff781cfe00 INFO                GST_PADS gstpad.c:2590:gst_pad_link_full: linked v4l2src0:src and capsfilter0:sink, successful
0:00:00.379611500 94448 0xffff781cfe00 INFO               GST_EVENT gstevent.c:1660:gst_event_new_reconfigure: creating reconfigure event
0:00:00.379685500 94448 0xffff781cfe00 INFO               GST_EVENT gstpad.c:5946:gst_pad_send_event_unchecked:<v4l2src0:src> Received event on flushing pad. Discarding
0:00:00.379844000 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstutils.c:1816:gst_element_link_pads_full: trying to link element capsfilter0:src to element appsink0:(any)
0:00:00.379952625 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:1016:gst_element_get_static_pad: found pad capsfilter0:src
0:00:00.380072125 94448 0xffff781cfe00 INFO                GST_PADS gstutils.c:1079:gst_pad_check_link: trying to link capsfilter0:src and appsink0:sink
0:00:00.380371125 94448 0xffff781cfe00 INFO                GST_PADS gstutils.c:1632:prepare_link_maybe_ghosting: capsfilter0 and appsink0 in same bin, no need for ghost pads
0:00:00.380522250 94448 0xffff781cfe00 INFO                GST_PADS gstpad.c:2382:gst_pad_link_prepare: trying to link capsfilter0:src and appsink0:sink
0:00:00.380725250 94448 0xffff781cfe00 INFO                GST_PADS gstpad.c:2590:gst_pad_link_full: linked capsfilter0:src and appsink0:sink, successful
0:00:00.380802125 94448 0xffff781cfe00 INFO               GST_EVENT gstevent.c:1660:gst_event_new_reconfigure: creating reconfigure event
0:00:00.380887375 94448 0xffff781cfe00 INFO               GST_EVENT gstpad.c:5946:gst_pad_send_event_unchecked:<capsfilter0:src> Received event on flushing pad. Discarding
0:00:00.381162250 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:1016:gst_element_get_static_pad: found pad appsink0:sink
0:00:00.381603500 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<appsink0> current NULL pending VOID_PENDING, desired next READY
0:00:00.381721375 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<appsink0> completed state change to READY
0:00:00.381846125 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<appsink0> notifying about state-changed NULL to READY (VOID_PENDING pending)
0:00:00.382106625 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'appsink0' changed state to 2(READY) successfully
0:00:00.382227125 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current NULL pending VOID_PENDING, desired next READY
0:00:00.382312500 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to READY
0:00:00.382398000 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed NULL to READY (VOID_PENDING pending)
0:00:00.382505125 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 2(READY) successfully
0:00:00.382599000 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<v4l2src0> current NULL pending VOID_PENDING, desired next READY
invoke, input sum 54961436
Sum of pixels in the latest frame 2: 12251
invoke, input sum 55065912
0:00:00.515320375 94448 0xffff781cfe00 INFO                    v4l2 v4l2_calls.c:588:gst_v4l2_open:<v4l2src0:src> Opened device 'XYGD Camera: XYGD Camera' (/dev/videoFRONT) successfully
0:00:00.515769125 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<v4l2src0> completed state change to READY
0:00:00.515896500 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed NULL to READY (VOID_PENDING pending)
0:00:00.516104000 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 2(READY) successfully
0:00:00.516472000 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2778:gst_element_continue_state:<pipeline0> committing state from NULL to READY, pending PLAYING, next PAUSED
0:00:00.516824250 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<pipeline0> notifying about state-changed NULL to READY (PLAYING pending)
0:00:00.517029375 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2786:gst_element_continue_state:<pipeline0> continue state change READY to PAUSED, final PLAYING
0:00:00.517435000 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<appsink0> current READY pending VOID_PENDING, desired next PAUSED
0:00:00.517666750 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2935:gst_bin_change_state_func:<pipeline0> child 'appsink0' is changing state asynchronously to PAUSED
0:00:00.517890125 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current READY pending VOID_PENDING, desired next PAUSED
0:00:00.518086000 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to PAUSED
0:00:00.518341500 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:00.518657250 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 3(PAUSED) successfully
0:00:00.518838750 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<v4l2src0> current READY pending VOID_PENDING, desired next PAUSED
0:00:00.519254000 94448 0xffff781cfe00 INFO                 basesrc gstbasesrc.c:1430:gst_base_src_do_seek:<v4l2src0> seeking: time segment start=0:00:00.000000000, offset=0:00:00.000000000, stop=99:99:99.999999999, rate=1.000000, applied_rate=1.000000, flags=0x00, time=0:00:00.000000000, base=0:00:00.000000000, position 0:00:00.000000000, duration 99:99:99.999999999
0:00:00.520841875 94448 0xffff781cfe00 INFO                    task gsttask.c:516:gst_task_set_lock: setting stream lock 0xffff793f2140 on task 0xffff50901050
0:00:00.521176500 94448 0xffff781cfe00 INFO                GST_PADS gstpad.c:6291:gst_pad_start_task:<v4l2src0:src> created task 0xffff50901050
0:00:00.522258500 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<v4l2src0> completed state change to PAUSED
0:00:00.522535000 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:00.522623625 94448 0xffff619a4860 INFO        GST_ELEMENT_PADS gstelement.c:1013:gst_element_get_static_pad: no such pad 'sink' in element "v4l2src0"
0:00:00.522858125 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2971:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 3(PAUSED) successfully without preroll
0:00:00.523078875 94448 0xffff781cfe00 INFO                pipeline gstpipeline.c:533:gst_pipeline_change_state:<pipeline0> pipeline is live
0:00:00.523435000 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2778:gst_element_continue_state:<pipeline0> committing state from READY to PAUSED, pending PLAYING, next PLAYING
0:00:00.523500750 94448 0xffff619a4860 INFO                 v4l2src gstv4l2src.c:550:gst_v4l2src_query_preferred_size:<v4l2src0> Detect input 0 as `Camera 1`
0:00:00.523583250 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<pipeline0> notifying about state-changed READY to PAUSED (PLAYING pending)
0:00:00.523799875 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2786:gst_element_continue_state:<pipeline0> continue state change PAUSED to PLAYING, final PLAYING
0:00:00.523857625 94448 0xffff619a4860 INFO                    v4l2 gstv4l2object.c:1241:gst_v4l2_object_fill_format_list:<v4l2src0:src> got 2 format(s):
0:00:00.524240000 94448 0xffff619a4860 INFO                    v4l2 gstv4l2object.c:1245:gst_v4l2_object_fill_format_list:<v4l2src0:src>   YUYV
0:00:00.524413000 94448 0xffff619a4860 INFO                    v4l2 gstv4l2object.c:1245:gst_v4l2_object_fill_format_list:<v4l2src0:src>   MJPG
0:00:00.524410250 94448 0xffff781cfe00 INFO               GST_EVENT gstevent.c:1530:gst_event_new_latency: creating latency event 0:00:00.000000000
0:00:00.524777375 94448 0xffff781cfe00 INFO                     bin gstbin.c:2759:gst_bin_do_latency_func:<pipeline0> configured latency of 0:00:00.000000000
0:00:00.525012000 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<appsink0> current READY pending PAUSED, desired next PLAYING
0:00:00.525226375 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2935:gst_bin_change_state_func:<pipeline0> child 'appsink0' is changing state asynchronously to PLAYING
0:00:00.525407500 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current PAUSED pending VOID_PENDING, desired next PLAYING
0:00:00.525527625 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<capsfilter0> completed state change to PLAYING
0:00:00.525656875 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<capsfilter0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.525884000 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 4(PLAYING) successfully
0:00:00.526082125 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<v4l2src0> completed state change to PLAYING
0:00:00.526211750 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<v4l2src0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.526422125 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 4(PLAYING) successfully
0:00:00.526642625 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2069:gst_bin_get_state_func:<pipeline0> getting state
0:00:00.526773125 94448 0xffff781cfe00 INFO              GST_STATES gstelement.c:2522:gst_element_get_state_func:<pipeline0> waiting for element to commit state
0:00:00.527140250 94448 0xffff619a4860 INFO                    v4l2 gstv4l2object.c:4752:gst_v4l2_object_probe_caps:<v4l2src0:src> probed caps: video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)720, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction)10/1; video/x-raw, format=(string)YUY2, width=(int)960, height=(int)540, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 20/1, 15/1, 10/1 }; video/x-raw, format=(string)YUY2, width=(int)720, height=(int)480, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 25/1, 20/1, 15/1, 10/1 }; video/x-raw, format=(string)YUY2, width=(int)812, height=(int)420, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 25/1, 20/1, 15/1, 10/1 }; image/jpeg, width=(int)1280, height=(int)720, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 60/1, 30/1, 25/1 }; image/jpeg, width=(int)960, height=(int)540, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 60/1, 30/1, 25/1 }; image/jpeg, width=(int)720, height=(int)480, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 60/1, 30/1, 25/1 }; image/jpeg, width=(int)812, height=(int)420, pixel-aspect-ratio=(fraction)1/1, framerate=(fraction){ 60/1, 30/1, 25/1 }
Sum of pixels in the latest frame 2: 12251
0:00:00.547849875 94448 0xffff619a4860 INFO                 v4l2src gstv4l2src.c:647:gst_v4l2src_negotiate:<v4l2src0> fixated to: video/x-raw, format=(string)YUY2, width=(int)812, height=(int)420, framerate=(fraction)25/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)2:4:5:1
0:00:00.548538875 94448 0xffff619a4860 INFO               GST_EVENT gstevent.c:892:gst_event_new_caps: creating caps event video/x-raw, format=(string)YUY2, width=(int)812, height=(int)420, framerate=(fraction)25/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)2:4:5:1
0:00:00.548959625 94448 0xffff619a4860 INFO           basetransform gstbasetransform.c:1325:gst_base_transform_setcaps:<capsfilter0> reuse caps
0:00:00.549235750 94448 0xffff619a4860 INFO               GST_EVENT gstevent.c:892:gst_event_new_caps: creating caps event video/x-raw, format=(string)YUY2, width=(int)812, height=(int)420, framerate=(fraction)25/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)2:4:5:1
0:00:00.549558500 94448 0xffff619a4860 INFO               GST_EVENT gstevent.c:892:gst_event_new_caps: creating caps event video/x-raw, format=(string)YUY2, width=(int)812, height=(int)420, framerate=(fraction)25/1, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)2:4:5:1
invoke, input sum 55089027
0:00:00.587377125 94448 0xffff619a4860 INFO                    v4l2 gstv4l2object.c:4083:gst_v4l2_object_set_format_full:<v4l2src0:src> Set capture framerate to 25/1
0:00:00.587530875 94448 0xffff619a4860 INFO                    v4l2 gstv4l2object.c:3251:gst_v4l2_object_setup_pool:<v4l2src0:src> accessing buffers via mode 2
0:00:00.588640875 94448 0xffff619a4860 INFO          v4l2bufferpool gstv4l2bufferpool.c:604:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> increasing minimum buffers to 2
0:00:00.588834500 94448 0xffff619a4860 INFO          v4l2bufferpool gstv4l2bufferpool.c:617:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> reducing maximum buffers to 32
0:00:00.589517250 94448 0xffff619a4860 INFO          v4l2bufferpool gstv4l2bufferpool.c:617:gst_v4l2_buffer_pool_set_config:<v4l2src0:pool0:src> reducing maximum buffers to 32
0:00:00.592832375 94448 0xffff619a4860 WARN          v4l2bufferpool gstv4l2bufferpool.c:884:gst_v4l2_buffer_pool_start:<v4l2src0:pool0:src> Uncertain or not enough buffers, enabling copy threshold
Sum of pixels in the latest frame 2: 12251
invoke, input sum 55026501
Sum of pixels in the latest frame 2: 12251
invoke, input sum 55091355
Sum of pixels in the latest frame 2: 12251
0:00:00.832698625 94448 0xffff619a4860 INFO               GST_EVENT gstevent.c:972:gst_event_new_segment: creating segment event time segment start=0:00:00.000000000, offset=0:00:00.000000000, stop=99:99:99.999999999, rate=1.000000, applied_rate=1.000000, flags=0x00, time=0:00:00.000000000, base=0:00:00.000000000, position 0:00:00.000000000, duration 99:99:99.999999999
0:00:00.832894875 94448 0xffff619a4860 INFO                 basesrc gstbasesrc.c:3018:gst_base_src_loop:<v4l2src0> marking pending DISCONT
0:00:00.833110500 94448 0xffff619a4860 INFO              GST_STATES gstbin.c:3406:bin_handle_async_done:<pipeline0> setting state from PAUSED to PAUSED, pending PLAYING
0:00:00.833233125 94448 0xffff619a4860 INFO              GST_STATES gstbin.c:3428:bin_handle_async_done:<pipeline0> continue state change, pending PLAYING
0:00:00.833972375 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:3224:gst_bin_continue_func:<pipeline0> continue state change PAUSED to PLAYING, final PLAYING
0:00:00.834252250 94448 0xffff619a4060 INFO               GST_EVENT gstevent.c:1530:gst_event_new_latency: creating latency event 0:00:00.060000000
0:00:00.834474000 94448 0xffff619a4060 INFO                     bin gstbin.c:2759:gst_bin_do_latency_func:<pipeline0> configured latency of 0:00:00.060000000
0:00:00.834652125 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<appsink0> current PAUSED pending VOID_PENDING, desired next PLAYING
0:00:00.834771250 94448 0xffff619a4060 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<appsink0> completed state change to PLAYING
0:00:00.834887000 94448 0xffff619a4060 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<appsink0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
invoke, input sum 55027005
0:00:00.835050875 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'appsink0' changed state to 4(PLAYING) successfully
0:00:00.835177250 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<capsfilter0> current PLAYING pending VOID_PENDING, desired next PLAYING
0:00:00.835359125 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2597:gst_bin_element_set_state:<capsfilter0> skipping transition from PLAYING to  PLAYING
0:00:00.835518375 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'capsfilter0' changed state to 4(PLAYING) successfully
0:00:00.835621375 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2479:gst_bin_element_set_state:<v4l2src0> current PLAYING pending VOID_PENDING, desired next PLAYING
0:00:00.835725875 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2597:gst_bin_element_set_state:<v4l2src0> skipping transition from PLAYING to  PLAYING
0:00:00.835811375 94448 0xffff619a4060 INFO              GST_STATES gstbin.c:2928:gst_bin_change_state_func:<pipeline0> child 'v4l2src0' changed state to 4(PLAYING) successfully
0:00:00.835946125 94448 0xffff619a4060 INFO              GST_STATES gstelement.c:2806:gst_element_continue_state:<pipeline0> completed state change to PLAYING
0:00:00.836103750 94448 0xffff619a4060 INFO              GST_STATES gstelement.c:2706:_priv_gst_element_state_changed:<pipeline0> notifying about state-changed PAUSED to PLAYING (VOID_PENDING pending)
0:00:00.836392750 94448 0xffff781cfe00 INFO        GST_ELEMENT_PADS gstelement.c:1016:gst_element_get_static_pad: found pad appsink0:sink
[ WARN:[email protected]] global /usr/src/debug/opencv/4.6.0.imx-r0/git/modules/videoio/src/cap_gstreamer.cpp (1405) open OpenCV | GStreamer warning: Cannot query video position: status=0, value=-1, duration=-1
done open 
Camera opened successfully.
0:00:00.837683125 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2069:gst_bin_get_state_func:<pipeline0> getting state
cap cnls: 2 w 812 420
0:00:00.840251500 94448 0xffff781cfe00 INFO              GST_STATES gstbin.c:2069:gst_bin_get_state_func:<pipeline0> getting state
Sum of pixels in the latest frame 2: 12251
0:00:00.872442250 94448 0xffff619a4860 WARN                 v4l2src gstv4l2src.c:1123:gst_v4l2src_create:<v4l2src0> lost frames detected: count = 1 - ts: 0:00:00.311987500


0 Kudos
Reply
4 Replies

2,060 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please provide the code to tested since you are using gstreamer with npu and camera. Also you can check the machine learning guide:

https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf

Regards

 

0 Kudos
Reply

2,052 Views
RIMASTA
Contributor I

I provide code. I do not know if you are building using yocto or sdk generated from yocto. 
You will need to link to imx-tensorflow and opencv:


These are found in the imx-tensorflow branch lf-5.10.52_2.1.0,  repo as described in the machine learning user guide:

add_executable(SOME_NAME path/bug.cpp
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/tools/delegates/default_execution_provider.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/tools/delegates/delegate_provider.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/tools/tool_params.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/nnapi/sl/SupportLibrary.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/nnapi/nnapi_implementation.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/nnapi/nnapi_util.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/tools/delegates/nnapi_delegate_provider.cc
${TENSORFLOW_SOURCE_DIR}/tensorflow/lite/tools/delegates/xnnpack_delegate_provider.cc
)
0 Kudos
Reply

2,027 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it looks like the npu is not executed, will see with the developers thanks for the catch!

Regards

0 Kudos
Reply

1,978 Views
RIMASTA
Contributor I

Thanks, My workaround is v4l2, but Since root cause is not known I am forced to ship code to product with a potential bug. Anyway in case you find the root cause, please let me know even if you do not have a fix since I want more confidence that v4l2 is a good workaround.

0 Kudos
Reply