IMX8MP L5.4.70-2.3.0 image have some bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MP L5.4.70-2.3.0 image have some bug

722件の閲覧回数
coindu
Contributor IV
Hi: I have a IMX8MP evk board . When I download the L5.4.70 image and burn it to the development board,then some bugs have occurred. 1,HDMI display will show a red column line on the left. If plug in HDMI cable or wake up from standby. 2, pcie cannot detect device MD5SUM:19b64eb1225c7e39e9174afca6dc2225 L5.4.70-2.3.0_images_MX8MPEVK.zip In fact, the image compiled with L5.4.3 BSP does not have these problems. Is the L5.4.70 version not tested? not a GA version?
0 件の賞賛
返信
1 返信

713件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

I didn't represent these bugs in images made from this version bsp.

Can you provide the error log?

The new version bsp L5.10.9_1.0.0 will be released these days, you can try this version.

0 件の賞賛
返信