IMX8MP DDR Stress Tool Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP DDR Stress Tool Error

2,848 Views
abhiroopnray
Contributor III

I am trying to boot a custom IMX8MP Board.

I have made the pin configuration changes in the LPDDR4_RPA excel file and trying to calibrate and run DDR Stress test using MScale DDR Tool.

I am getting the following:

1> When I click download with the .ds file:

Download is complete
Waiting for the target board boot...

===================hardware_init=====================


********Found PMIC PCA9450**********
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:52:12
*************************************************************************

Waiting for board configuration from PC-end...

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x97d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 1800MHz
DDR Clock: 2000MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 17, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 3072MB
Density per controller is: 6144MB
Total density detected on the board is: 6144MB
============================================

MX8M-plus: Cortex-A53 is found

*************************************************************************

 

2> When I press calibrate:

============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @2000Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @200Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @50Mhz...
[Process] End of CA training
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 2D-Training @2000Mhz...
[Process] End of initialization
[Process] End of 2D write delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D read delay/voltage center optimization
[Result] PASS

============ Step 2: DDR memory accessing... ============
Verifying DDR frequency [email protected]
Verifying DDR frequency [email protected]
Verifying DDR frequency [email protected]
[Result] OK

3> When I press Stress test with all default configuration: 

============ Step 3: DDR parameters processing... ============
[Result] Done

Success: DDR Calibration completed!!!
DDR Stress Test Iteration 1
--------------------------------
--Running DDR test on region 1--
--------------------------------

t0.1: data is addr test
...Address of failure: 0x0000000101E00000
Data read was: 0x0000FFFF41E0FFFF
But pattern was: 0x0000000041E00000

I am unsure about the error. Can anyone please tell me what this error is? Will the board be able to boot after this ?



Tags (2)
0 Kudos
Reply
3 Replies

2,786 Views
abhiroopnray
Contributor III

Hello,

May I know, when can I get a response?

0 Kudos
Reply

2,728 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Did your board work well now? If no, you can share us your script and ddr section schematic to us, we will help check.

Wish you have a nice day

0 Kudos
Reply

2,719 Views
abhiroopnray
Contributor III

Hello,

Thank you for your response.

The board is working if I set the lpddr4 Clock frequency to 800MHz or 1200MHz. The above error persists when I set clock frequency to 2000MHz.

 

For 800MHz:

memory set0x30360054320x7D060

 

For 1200MHz:

memory set0x30360054320xC8022

 

For 2000MHz:

memory set0x30360054320xFA031

 

Can you please tell me do I need to make any other change for 2000MHz?

0 Kudos
Reply