IMX8MP DART board WIFI bringup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MP DART board WIFI bringup

1,202 次查看
khajiit
Contributor I

I am trying to get wifi working on the DART-MX8M-PLUS with Yocoto Scarthgap. I noticed in the demo image that variscite provides there are kernel objects called moal.ko and mlan.ko which are not being built into my custom image even though I have the variscite layers, so I think I might need to include more of the recipes. How can I get these modules to build into the yocto image? Are there any other recipes that are needed to be included into the build for wifi to automatically work at boot?

 

Thanks

 

 

0 项奖励
回复
2 回复数

1,183 次查看
khajiit
Contributor I

I have gotten the moal and mlan drivers to show up which has made the wlan0 network interface show up as well, allowing me to get wifi to connect. The only thing now is that there is an error repeatedly printed: "ERR: Role is AP"

0 项奖励
回复

1,178 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to contact DART.

Regards

0 项奖励
回复