IMX8MP DART board WIFI bringup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP DART board WIFI bringup

1,206 Views
khajiit
Contributor I

I am trying to get wifi working on the DART-MX8M-PLUS with Yocoto Scarthgap. I noticed in the demo image that variscite provides there are kernel objects called moal.ko and mlan.ko which are not being built into my custom image even though I have the variscite layers, so I think I might need to include more of the recipes. How can I get these modules to build into the yocto image? Are there any other recipes that are needed to be included into the build for wifi to automatically work at boot?

 

Thanks

 

 

0 Kudos
Reply
2 Replies

1,187 Views
khajiit
Contributor I

I have gotten the moal and mlan drivers to show up which has made the wlan0 network interface show up as well, allowing me to get wifi to connect. The only thing now is that there is an error repeatedly printed: "ERR: Role is AP"

0 Kudos
Reply

1,182 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to contact DART.

Regards

0 Kudos
Reply