IMX8MP 2GB RAM Support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP 2GB RAM Support.

3,307 Views
Athi
Contributor I

 We are facing a problem in our board which was developed based on the IMX8MP board. We got a patch from NXP to modify the BSP for 2GB board and it is working for W21H2-1-3-0 BSP. Then we tried this patch in Windows 10 IoT BSP W21H2-1-4-1 but the board is not booting now with this patch. Is there any new patch?

IMX8MPLUS 

 

0 Kudos
Reply
4 Replies

3,204 Views
Athi
Contributor I

Hi @Bio_TICFSL , Is there any update?

0 Kudos
Reply

3,206 Views
Athi
Contributor I

Hi @Bio_TICFSL ,  Is there any update on this?

0 Kudos
Reply

3,281 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it works with linux BSP it does not with windows you need a new version of windows to support wifi.

Regards

0 Kudos
Reply

3,252 Views
Athi
Contributor I

Hi @Bio_TICFSL , We got patch from NXP for Windows 10 IoT W21H2-1-3-0 BSP only and it is working. We have tried this patch in Windows 10 IoT BSP W21H2-1-4-1 but the board is not booting.

IMX8MP RAM ISSUE - NXP Community  - This is previously we have addressed.

0 Kudos
Reply