[IMX8MNDDR3L] Cannot flash with uuu using kirkstone BSP (Failed to configure default pinctrl)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[IMX8MNDDR3L] Cannot flash with uuu using kirkstone BSP (Failed to configure default pinctrl)

Jump to solution
1,012 Views
Krisna
Contributor II

Hi there,

We have tried to generate IMX8MN image using zeus BSP, so far so good, but because it's already reach EOL, we plan to migrate to kirkstone BSP.

We use this xml to sync the sources:

$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.0.0.xml

 

And we use these commands to build the image:

$ MACHINE=imx8mnddr3levk DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b build
$ bitbake core-image-minimal

 

We manage to build the image, but when we tried to flash it to 8MNANOD3L-EVK using uuu, it always stuck here:

 

uuu perspective:

C:\Work\Shared>uuu.exe -V -b emmc_all imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk core-image-minimal-imx8mnddr3levk.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.165-0-ge10b026

Build in config:
        Pctl     Chip            Vid     Pid     BcdVersion
        ==================================================
        SDPS:    MX8QXP          0x1fc9  0x012f  [0x0002..0xffff]
        SDPS:    MX8QM           0x1fc9  0x0129  [0x0002..0xffff]
        SDPS:    MX8DXL          0x1fc9  0x0147
        SDPS:    MX28            0x15a2  0x004f
        SDPS:    MX815           0x1fc9  0x013e
        SDPS:    MX865           0x1fc9  0x0146
        SDPS:    MX8ULP          0x1fc9  0x014a
        SDPS:    MX8ULP          0x1fc9  0x014b
        SDP:     MX7D            0x15a2  0x0076
        SDP:     MX6Q            0x15a2  0x0054
        SDP:     MX6D            0x15a2  0x0061
        SDP:     MX6SL           0x15a2  0x0063
        SDP:     MX6SX           0x15a2  0x0071
        SDP:     MX6UL           0x15a2  0x007d
        SDP:     MX6ULL          0x15a2  0x0080
        SDP:     MX6SLL          0x1fc9  0x0128
        SDP:     MX7ULP          0x1fc9  0x0126
        SDP:     MXRT106X        0x1fc9  0x0135
        SDP:     MX8MM           0x1fc9  0x0134
        SDP:     MX8MQ           0x1fc9  0x012b
        SDPU:    SPL             0x0525  0xb4a4  [0x0000..0x04ff]
        SDPV:    SPL1            0x0525  0xb4a4  [0x0500..0x9998]
        SDPU:    SPL             0x0525  0xb4a4  [0x9999..0x9999]
        SDPU:    SPL             0x3016  0x1001  [0x0000..0x04ff]
        SDPV:    SPL1            0x3016  0x1001  [0x0500..0x9998]
        FBK:                     0x066f  0x9afe
        FBK:                     0x066f  0x9bff
        FB:                      0x0525  0xa4a5
        FB:                      0x18d1  0x0d02
        FB:                      0x3016  0x0001

Run built-in script:

uuu_version 1.4.149

# @_flash.bin            | bootloader, which can extract from wic image
# @_image   [_flash.bin] | wic image burn to emmc.


# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -scanterm -f imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk -skipspl -scanterm
SDPV: jump
# }


FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all core-image-minimal-imx8mnddr3levk.wic
FB: flash -scanterm bootloader imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done


Wait for Known USB Device Appear...
New USB Device Attached at 2:34
2:34>Start Cmd:SDPS: boot -scanterm -f imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk
99%libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] The device is not connected.
2:34>Okay (2.949s)

 

U-boot perspective:

U-Boot SPL 2022.04-lf_v2022.04+g1c881f4da8 (Jun 07 2022 - 05:16:02 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 1600MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
Trying to boot from BOOTROM
Find img info 0x&480319a0, size 1080
Need continue download 1024
Download 1410960, Total size 1412592
NOTICE:  BL31: v2.6(release):lf-5.15.32-2.0.0-0-gc6a19b1a3
NOTICE:  BL31: Built : 06:37:22, Jun  7 2022


U-Boot 2022.04-lf_v2022.04+g1c881f4da8 (Jun 07 2022 - 05:16:02 +0000)

CPU:   i.MX8MNano UltraLite Quad rev1.0 1400 MHz (running at 1200 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 40C
Reset cause: POR
Model: NXP i.MX8MNano DDR3L EVK board
DRAM:  992 MiB
TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
Core:  149 devices, 21 uclasses, devicetree: separate
MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from nowhere... OK
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated

 BuildInfo:
  - ATF c6a19b1

MMC: no card present
Detect USB boot. Will enter fastboot mode!
Net:   eth0: ethernet@30be0000
Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for                                mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot:  0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
Failed to configure default pinctrl

 

Using zeus BSP, we never encounter such issue. And we find that sd.bin size is quite small on kirkstone (1.732 KB) compare to zeus (3.184 KB). Any hint would be appreciated. Thank you for your time and support.

Labels (1)
0 Kudos
Reply
1 Solution
981 Views
Krisna
Contributor II

Hi there,

After troubleshooting the whole day, found out that I need to change /build/tmp/work/imx8mnddr3levk-poky-linux/u-boot-imx/2022.04-r0/build/imx8mn_ddr3l_evk_config/.config

CONFIG_USB_GADGET_VENDOR_NUM=0x1fc9
CONFIG_USB_GADGET_PRODUCT_NUM=0x0152

to:

CONFIG_USB_GADGET_VENDOR_NUM=0x0525
CONFIG_USB_GADGET_PRODUCT_NUM=0xa4a5

And call:

bitbake u-boot-imx -c compile -f
bitbake core-image-minimal -f

Now I can use flash with uuu + u-boot without problem. I consider it to be a BSP bug though, hopefully it can be resolved on next released. Thanks.

View solution in original post

0 Kudos
Reply
1 Reply
982 Views
Krisna
Contributor II

Hi there,

After troubleshooting the whole day, found out that I need to change /build/tmp/work/imx8mnddr3levk-poky-linux/u-boot-imx/2022.04-r0/build/imx8mn_ddr3l_evk_config/.config

CONFIG_USB_GADGET_VENDOR_NUM=0x1fc9
CONFIG_USB_GADGET_PRODUCT_NUM=0x0152

to:

CONFIG_USB_GADGET_VENDOR_NUM=0x0525
CONFIG_USB_GADGET_PRODUCT_NUM=0xa4a5

And call:

bitbake u-boot-imx -c compile -f
bitbake core-image-minimal -f

Now I can use flash with uuu + u-boot without problem. I consider it to be a BSP bug though, hopefully it can be resolved on next released. Thanks.

0 Kudos
Reply