IMX8MN Cortex-M7 ECSPI with SDMA - SDMA interrupt is generated before transmission

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MN Cortex-M7 ECSPI with SDMA - SDMA interrupt is generated before transmission

1,166 次查看
okobelnc
Contributor I

Hi. I am using IMX8MN cortex-m7 core, and want to use the ECSPI2 peripheral as a SPI master with SDMA.

 

I see that a lot of times, the SDMA1 interrupt for the TX channel is generated in the middle of ECSPI_MasterTransferSDMA, right after its call to SDMA_ConfigBufferDescriptor:

okobelnc_0-1726396533615.png

okobelnc_1-1726396563063.png

Since the interrupt is generated at this moment before starting the transmission, the 

SDMA_EcspiMasterCallback callback disables the ECSPI peripheral and the transmission and aborts all the SPI transaction before it started.
 
Here is my ECSPI and DMA configuration:
 
typedef union
{
    ecspi_master_config_t tMasterConfig;
    ecspi_slave_config_t tSlaveConfig;
}CTHAL_SPI_NXP_FSL_Config_t;
 
#define UNUSED_CFG                        (0)
#define NETX90_CS_GPIO_PORT               (GPIO5)
#define NETX90_CS_PIN_NUM                 (13)
#define NETX90_SPI_PERIPHERAL             (ECSPI2)
#define NETX90_SPI_PERIPHERAL_SRC_CLK_HZ  (80000000) /*!< 80MHz is the source clock of the ECSPI2 peripheral */
#define ONE_BYTE_BURST_LENGTH             (8)
#define NETX90_SPI_BAUDRATE_BPS           (23000000) /*!< 23MHz CLK */
#define SPI_CS_NO_DELAY                   (0)
#define SPI_SAMPLE_PERIOD_0               (0)
#define SPI_TX_FIFO_THRESHOLD             (1)
#define SPI_RX_FIFO_THRESHOLD             (0)
#define NETX90_SPI_SDMA_PERIPHERAL        (SDMAARM1) /*!< ECSPI2 DMA is supported only by SDMA1 */
#define INIT_STRUCT_ZEROS                 {0}
#define NETX90_SPI_SDMA_RX_CHANNEL        (1)
#define NETX90_SPI_SDMA_TX_CHANNEL        (2)
#define NETX90_SPI_SDMA_RX_CH_PRIO        (3)
#define NETX90_SPI_SDMA_TX_CH_PRIO        (2)
#define NETX90_SPI_EVT_SRC_TX             (3)       /*!< According to the reference manual -  ECSPI2 Tx request */
#define NETX90_SPI_EVT_SRC_RX             (2)       /*!< According to the reference manual -  ECSPI2 Rx request */
 
static CTHAL_SPI_NXP_FSL_Config_t s_tNetX90_SPI_Cfg =
{
    .tMasterConfig =
    {
        .channel = kECSPI_Channel0,
        .burstLength = ONE_BYTE_BURST_LENGTH,
        .samplePeriodClock = kECSPI_spiClock,
        .baudRate_Bps = NETX90_SPI_BAUDRATE_BPS,
        .chipSelectDelay = SPI_CS_NO_DELAY,
        .samplePeriod = SPI_SAMPLE_PERIOD_0,
        .txFifoThreshold = SPI_TX_FIFO_THRESHOLD,
        .rxFifoThreshold = SPI_RX_FIFO_THRESHOLD,
        .enableLoopback = false,
        .channelConfig = {
            .channelMode = kECSPI_Master,
            .clockInactiveState = kECSPI_ClockInactiveStateLow,
            .dataLineInactiveState = kECSPI_DataLineInactiveStateLow,
            .chipSlectActiveState = kECSPI_ChipSelectActiveStateLow,
            .phase = kECSPI_ClockPhaseSecondEdge,
            .polarity = kECSPI_PolarityActiveLow,
        },
    },
};
 
static sdma_config_t s_tNetX90_SPI_SDMA_Cfg =
{
    .enableRealTimeDebugPin = false,
    .isSoftwareResetClearLock = true,
    .ratio = kSDMA_HalfARMClockFreq,
};

static CTHAL_SPI_NXP_FSL_SDMA_Handles_t s_tNetX90_SPI_SDMA_Handles __attribute__((aligned(4))) =
{
    .tSDMATXHandle = INIT_STRUCT_ZEROS,
    .tSDMARXHandle = INIT_STRUCT_ZEROS,
};

static CTHAL_SPI_NXP_FSL_SDMA_Context_Data_t s_tNetX90_SPI_SDMA_Context_Data __attribute__((aligned(4)))  =
{
    .tSDMATXContextData = INIT_STRUCT_ZEROS,
    .tSDMARXContextData = INIT_STRUCT_ZEROS,
};

static CTHAL_SPI_NXP_FSL_DMA_Cfg_t  s_tNetX90_SPI_DMA_Cfg __attribute__((aligned(4))) =
{
    .ptSDMAConfig = &s_tNetX90_SPI_SDMA_Cfg,
    .ptSDMAAddr = SDMAARM1,
    .ptSDMAHandles = &s_tNetX90_SPI_SDMA_Handles,
    .ptSDMAContextData = &s_tNetX90_SPI_SDMA_Context_Data,
    .ulTXDMAChannelNum = NETX90_SPI_SDMA_TX_CHANNEL,
    .ulRXDMAChannelNum = NETX90_SPI_SDMA_RX_CHANNEL,
    .bTXDMAChannelPriority = NETX90_SPI_SDMA_TX_CH_PRIO,
    .bRXDMAChannelPriority = NETX90_SPI_SDMA_RX_CH_PRIO,
    .ulEventSourceTx = NETX90_SPI_EVT_SRC_TX,
    .ulEventSourceRx = NETX90_SPI_EVT_SRC_RX,
};

static CTHAL_SPI_NXP_FSL_ECSPI_Handle_t  s_tNetX90_SPI_Handle  __attribute__((aligned(4))) =
{
    .tSDMAHandle = INIT_STRUCT_ZEROS,
};
 
 
 
How can I resolve this issue?

 

Thanks,

Ofir

 

标签 (1)
0 项奖励
回复
1 回复

1,023 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I already follow your quesitons in the case you create.

0 项奖励
回复