hello,I use imx8mm android10,I only modified the SD card pins,uboot-imx/arch/arm/dts/imx8mm-evk.dts:
uboot Boot failure:
U-Boot 2020.04-dirty (Dec 07 2020 - 17:51:27 +0800)
CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 50C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
tcpc_init: Can't find device id=0x52
setup_typec: tcpc port2 init failed, err=-19
tcpc_init: Can't find device id=0x50
setup_typec: tcpc port1 init failed, err=-19
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment
[*]-Video Link 0Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22
[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22
In: serial
Out: serial
Err: serial
BuildInfo:
- ATF 0263634
- U-Boot 2020.04-dirty
flash target is MMC:1
Net:
Error: ethernet@30be0000 address not set.
Error: ethernet@30be0000 address not set.
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
avb_slot_verify.c:772: ERROR: vbmeta_a: Error loading vbmeta data.
verify FAIL, state: LOCK
Solved! Go to Solution.
The controller connected to the SDcard slot is set to work with Wi-Fi expansion card in Android10.0.0_2.5.0 demo image, it does not support to access SDcard.
so basically, if the dtbo image support Wi-Fi expansion card, then the images cannot boot up from SD card.
Could you tell us are you using the reference board or the board you design by yourself? And which andorid10 are you using?
Now I have the same problem with the official image,emmc is ok,Sd card prompts lock error。android-10.0.0_2.5.0_image_8mmevk.tar.gz imx8mm lpddr4 sd 32G EMMC16G。
android 9 is ok。linux 4.14.98 is ok。emmc and sd。
One more question:
Burn the image using uuu_imx_android_flash.bat,windows7/10 and ubuntu,There will be temporary files that cannot be deleted automatically and need to be manually deleted。 C:\Users\cjf\AppData\Local\Temp ,ubuntu ls /tmp/
The controller connected to the SDcard slot is set to work with Wi-Fi expansion card in Android10.0.0_2.5.0 demo image, it does not support to access SDcard.
so basically, if the dtbo image support Wi-Fi expansion card, then the images cannot boot up from SD card.
I used my own design board, referring to the IMX8mm EVK LPDDR4。it is android-10.0.0_2.5.0_image_8mmevk.tar.gz,Just a change in the SD card pin。
This android-10.0.0_2.3.0 version should be work. You can have a try.
hello
I want to use Android10_2.5.0,My wifi card is AP6255 BCM43455,How do I modify an dtbo image?Get rid of its own wifi card?
You can not use the demo images supply in our website, it's for the reference board.
You need to download the source and porting your wifi to your board.
Thank you. Can I remove the official wifi card?