IMX8M xtal bypass

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,355件の閲覧回数
GH
Contributor I

Hello,

I am designing a new board with the IMX8M on it and I'd like to use oscillators for the 25MHz and 27MHz inputs.  I see a hint that this is possible in the reference manual where it talks about bypass mode, but I don't see how to hook this up electrically.

1) Can I use an oscillator (1.8V output) as a clock for the IMX8M?

2) What exactly do I hook up to the XTAL1 and XTAL0 inputs for 25MHz and 27MHz?

3) Are there any other concerns with doing this? is there anything different that needs done in software for bootup?

 

Thanks!

0 件の賞賛
返信
1 解決策
2,338件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi GH,

 

    I discussed your question with i.MX expert team, it is not recommended that you use OSC for i.MX8MQ.

    In addition, the amplitude of 25MHz and 27MHz clock is not 1.8V, BUT 1.1V.

 

Hope above information is helpful to you.

Have a nice day!

B.R,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,329件の閲覧回数
GH
Contributor I

Weidong,

Thanks for the reply, I'll plan on using crystals instead.

have a good day!

0 件の賞賛
返信
2,339件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi GH,

 

    I discussed your question with i.MX expert team, it is not recommended that you use OSC for i.MX8MQ.

    In addition, the amplitude of 25MHz and 27MHz clock is not 1.8V, BUT 1.1V.

 

Hope above information is helpful to you.

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信