IMX8M's USB Port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M's USB Port

1,609 Views
xuyuanzhi
Contributor I

When download the Imx8m's Image, the Imx8m EVK board use the J901 USB TYPE-C conncector. I wonder when use the Mfgtool download the Image through this port , the usb is running USB2.0 or USB3.0?  When downloading Image, if only the usb1_dp and usb1_dn is needed, the other usb signals is not neceasary? Thank you!

Labels (1)
0 Kudos
Reply
1 Reply

1,352 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi xu,

When using i.MX8 EVK and the mfgtool use USB3.0.

Regards

0 Kudos
Reply