IMX8M mini MIPI_DSI DRM device not loading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M mini MIPI_DSI DRM device not loading

1,227件の閲覧回数
nivednk14
Contributor I

HI ,

We have custom IMX8M board with ILI9881C panel.

I have  Modified kconfig and compiled with ili988c Driver

I have also  Enabled ili device node in DTS

 

&mipi_dsi {
status = "okay";
panel1: panel@0 {
reg = <1>;
compatible = "bananapi,lhr050h41","ilitek,ili9881c";
reset-gpios = <&gpio3 12 1>;
power-supply = <&reg_mipi_phy>;
backlight = <&backlight>;
};

};

I don't see any kind of error while booting on drm/mipi/ or ili,

When i checked the code I could see that the device attach is not working properly saying that the drm_mipi bus has no device .

The device driver is unchanged . Only change I did was to enable it in dts.

root@imx8mm:~# dmesg |grep drm
[ 1.677021] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0
root@imx8mm:~#

0 件の賞賛
返信
1 返信

1,203件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi 

I need all changes you do, including your defconfig change, kconfig change

0 件の賞賛
返信