IMX8M-NANO 4.14.98-2.1.0 python3-sqlite3 doesn't work?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M-NANO 4.14.98-2.1.0 python3-sqlite3 doesn't work?

2,737件の閲覧回数
sergei_p
Contributor III

I'm working with IMX8M NANO EVK running 4.14.98-2.1.0 release and python3-sqlite3 doesn't seem work:

root@imx8mn:~# python3
Python 3.5.5 (default, Mar 10 2020, 00:13:12)
[GCC 7.3.0] on linux
Type "help", "copyright", "credits" or "license" for more information.
>>> import sqlite3
>>> conn = sqlite3.connect('example.db')
Traceback (most recent call last):
  File "<stdin>", line 1, in <module>
AttributeError: module 'sqlite3' has no attribute 'connect'

I checked and libsqlite3 package is installed on the filesystem.

Has anyone tried python3-sqlite3 there, or on any other platform, on any NXP Yocto release?

0 件の賞賛
返信
2 返答(返信)

2,618件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sergei,

You need python 3.6 to install sqlite3, in yocto you have python 3.5

Regards

0 件の賞賛
返信

2,618件の閲覧回数
sergei_p
Contributor III

Thanks.

You mean that the error has been fixed since the Yocto recipe for python3.6.

In fact, this particular commit from the poky repo does the fix:

commit f51d0a19afeb3cf9b5bad6e3b470b2a8fb6065f8
Author: Ross Burton <[email protected]>
Date: Fri Sep 28 17:06:14 2018 +0100

python3: move sqlite files into python-sqlite

sqlite3/__init__.py was accidentally included in python3-misc.

(From OE-Core rev: 4e397e16996662bce51608cf5e20448b9803c476)

Signed-off-by: Ross Burton <[email protected]>
Signed-off-by: Richard Purdie <[email protected]>

0 件の賞賛
返信