IMX8M Mini working with UART3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M Mini working with UART3

3,086件の閲覧回数
shai_b
Senior Contributor II

Dear team,

My customer is trying to use UART3 with our IMX8MM-EVK, as I know such changes need to be done within the device tree.

but since the customer needs to change such a small parameter he would like to know if there is an option to change the UART3 of imx8mm (based on Yocto 5.15x Multimedia image) via U-Boot?

looking for your kind support, thanks in advance 

KR,

Shai

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,063件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,982件の閲覧回数
shai_b
Senior Contributor II

Hi @Rita_Wang ,

The customer does not want to change the debug port, but only to add the option to enable the UART3 so he can work use it on the user space?

can you please send me an example of how to change the correct device tree file and enable the UART3 to be 'active'?

Wating for your kind feedback, Many thanks.

Shai

0 件の賞賛
返信

2,971件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Like this, you can ask customer to try

 

imx8mn-evk.dtsi
1. Remove UART2

pinctrl_uart3: uart3grp {
    fsl,pins = <
    MX8MN_IOMUXC_UART3_RXD_UART3_DCE_RX 0x140
    MX8MN_IOMUXC_UART3_TXD_UART3_DCE_TX 0x140
    >;
};

/*
&uart2 { 
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_uart2>;
    status = "okay";
};
*/

&uart3 { /*Console*/
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_uart3>;
    assigned-clocks = <&clk IMX8MN_CLK_UART3>;
    assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_80M>;
    /*fsl,uart-has-rtscts;*/  
    status = "okay";
};

2. changing uart2 to uart3
#include <dt-bindings/usb/pd.h>
#include "imx8mn.dtsi"

/ {
    chosen {
        stdout-path = &uart3;
    };

3,077件の閲覧回数
shai_b
Senior Contributor II

There is any update?

KR,

Shai

0 件の賞賛
返信